Part Number: CC2650STK
Hello,
I´m using the SensorTag board right now and wanted to test a external antenna of mine.
Below is a part of the sensortag schematic. I just removed the 0 Ohm resistor ANT5 and changed the coaxial switch J1 with an JSC connector.
I thought i would be done with it and the PCB antenna wouldnt be in use anymore. As it turns out the with no antenna connected (external) and the resistor removed i still get a signal on my phone (via the starter app for the sensortag). So somehow the antenna is still working. For further testing it is obviously quite hard to determine which antenna im measurring.
Does anyone have a clue what i did wrong? Do i even have to remove the ANT6 capacitor? Or something else completly?
Btw. the JSC connector is solder on correctly i did a few conductivity tests.
Many Regards,
looking forward for your good answers