Hello Everybody,
I'm facing an issue and I think I'm not the first to have this problem.
I'm using a CC2541 chip, mounted on a home made BLE module. I have to connect this module to a Rhode Schwartz CBT DB9.
To do this, I have loaded into the chip the CC2541_SmartRF_HostTestRelease_All.hex file, put an external power supply on the module, take the Rx, Tx, GND from my module, connect to an adapter UART/RS232, and then connect the adapter to the CBT. I put P0.4 to GND, to put the module in test mode. I have checked the CBT settings on TI wiki
It doesn't work and honestly I don't know why
Maybe someone can help me?
Best Regards,
Thomas