This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Issue

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640

Tool/software: Code Composer Studio

Environment:

simplelink_cc2640r2_sdk_1_40_00_45

Code Composer Studio 7.2.0.00013

SmartRF Flash Programmer 2 1.7.5

PCB with CC2640R2F

XDS200 USB Debug Probe

iPhone 7 with LightBlue App

I would like to connect my PCB CC2640R2F with the LightBlue App using simple_peripheral.

I have used CCS to build the simple_peripheral_cc2640r2lp_stack_library first, then the simple_peripheral_cc2640r2lp_app next.

The only modifications I make in CCS are to change the connection in properties to XDS 2xx USB Debug Probe, and change the build configuration to RCOSC.

I use the SmartRF Flash Programmer 2 ver. 1.7.5 to flash the .hex file using the XDS200 usb probe that is generated. (made under simple_peripheral_cc2640r2lp_app/FlashROM_StackLibrary_RCOSC/simple_peripheral_cc2640r2lp_app.hex)

Flash succeeds, but when I use the LightBlue App, nothing shows up under "Peripherals Nearby."

Is there something I am doing wrong here?

Thank you in advance.