This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: HOW can i configure CC2640 work on 2Mbps proprietary radio mode

Part Number: CC2640

hi , i want to configure cc2640 work on 2Mbps GFSK mode and write commond

CMD_PROP_RADIO_SETUP and CMD_FS

 as follow:

// Overrides for CMD_PROP_RADIO_SETUP
uint32_t pOverrides[] = {
        MCE_RFE_OVERRIDE(1,0,0,1,0,0),
        HW_REG_OVERRIDE(0x4038,0x34),
        HW_REG_OVERRIDE(0x6088,0x3F1F),
        HW_REG_OVERRIDE(0x608C,0x8213),
        HW32_ARRAY_OVERRIDE(0x405C,1),
        (uint32_t) 0x1801F800,
        HW32_ARRAY_OVERRIDE(0x402C,1),
        (uint32_t) 0x00608402,
        (uint32_t) 0xc0040031,
        (uint32_t) &shape[0],
        (uint32_t) 0x00000343,
        (uint32_t) 0x001000a3,
        (uint32_t) 0x000484a3,
        (uint32_t) 0x1c8f0583,
        (uint32_t) 0x1c8f0543,
        (uint32_t) 0x65980603,
        (uint32_t) 0x00020623,
        (uint32_t) 0x659805c3,
        (uint32_t) 0x000205e3,
        (uint32_t) 0x02010403,
        HW32_ARRAY_OVERRIDE(0x4034,1),
        (uint32_t) 0x177F0408,
        (uint32_t) 0x00008463,
        (uint32_t) 0x00388473,
        (uint32_t) 0x00F388a3,
        (uint32_t)0xFFFFFFFF,
};

// CMD_PROP_RADIO_SETUP
rfc_CMD_PROP_RADIO_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3806,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 200,
    .symbolRate.preScale = 12,
    .symbolRate.rateWord = 1048576, //symbolRate = (symbolRate.rateWord * 24000000)/(symbolRate.preScale * (2^20))
    .rxBw = 7,
    .preamConf.nPreamBytes = 0x8,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 16,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x0,
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .txPower = 0x9324,
    .pRegOverride = pOverrides,
};

// CMD_FS
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 2440,
    .fractFreq = 0x0000,
    .synthConf.bTxMode = 1,
    .synthConf.refFreq = 0x0,
};

when i send a package 

    RF_cmdPropTx.status = 0;
    RF_cmdPropTx.pktLen = len;
    RF_cmdPropTx.pPkt = (unsigned char *)bufPointer;
    HWREG(RFC_DBELL_BASE+RFC_DBELL_O_RFCPEIFG) = 0;
    RFCDoorbellSendTo((unsigned int)&(RF_cmdPropTx));
    while(0x3400 != RF_cmdPropTx.status); // wait for PROP_DONE_OK

it send ok and when i change len from 128 to 64,the task of time is decrease about 0.256ms,it seem that symbol rate set is OK,but in reciver device,it can't recive any package.

when i configure as followreciver device can recv package and work fine.

    .symbolRate.preScale = 15,
    .symbolRate.rateWord = 131072, //symbolRate = (symbolRate.rateWord * 24000000)/(symbolRate.preScale * (2^20))


i think maybe something configure error,and i want use SmartRF Studio 7 to export configure,but i can't find cc2640 proprietary mode .

can you help me,it stuck me a long time.