Part Number: LAUNCHXL-CC2640R2
Tool/software: TI-RTOS
Hi everyone,
As you know, bluetooth 5 is introduced and its coverage increases up to 200 meter with the help of the LE Coded Phy.
The difference between LE Coded Phy and standart LE Phy is that how many symbols you spend to code one data bit.
According to the Bluetooth specification, there are two type to encode the data which are 2 and 8 coding.
Here is the point that confuses my mind,
The LE Coded Phy property seems like a software trick to me because, there is no difference between sending data and sending coded data.
Instead of using CC2640R2 , can i use Bluetooth chips that support Bluetooth 4.2 to use LE Coded Phy.
Is it possible, if yes how can i do? if no what the physical layer changes on Bluetooth 5 ?
My second question is that;
In S=8 coding in LE Coded Phy, Transmitter will be in on 8 times higher than BLE 1M Phy. This will increase the power consumption of the transmitter.
Is there any work that show the increase in power consumption when S=8 LE Coded Phy is used compared to the BLE 1M Phy or can i say that the power consumption will increase 8 time?
Thanks for your attention
Have a nice day