Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640
Hello,
I'm wondering if two wire UART with power savings enabled on the CC2640R2F is possible?
From what I've been able to find, the procedure seems like it would be as follows:
1. Use this guide to add UART to your project. (SimpleBLEPeripheral for example)
1. a. The TL files supplied in the GIT link will need to be refactored to work with the current code base as events are used now instead of semaphores. Amongst other updates.
2. Replace the files in the project with the corresponding _swhs files from 
Is this basically what I would need to do to implement this?