This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: Change firmware to Hm-11

Part Number: CC2541
Other Parts Discussed in Thread: CC2540

Hi,

I am working on a prototype to scan BLE beacons.

At first, I used the HM-11 modules and everything works as I want. Except that I need external antenna so I can't use the HM-11 modules.
So I bought two different modules with a UFL connection using for the first the chip cc2540 (zbmodule) and for the second the chip cc2541 (module webee).
I would like to compile the firmware of the HM-11 on one of the modules with UFL connection.


I tried with the ccdebugger on the zbmodule, the flash procedure of the firmware works but I can't communicate to UART with the AT commands.
I also tried on the module webee but I can't start the flash procedure.

So, I'm wondering that it's possible to change firmware, may be that there is a procedure to totally reset the chip ? and then be able to change firmware?

Can you help me or is what the two module with external UFL is'nt compatible with that i want to do?

Thank you,