Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2640R2F
Hello,
I am using simple_peripheral on cc2640r2f. I tried to send notifications to Master but application was getting stop suddenly. While debugging i came to know that while sending the notification when the program enter
to following section :
if (GATT_Notification(connHandle, ¬i, FALSE) != SUCCESS)
{
GATT_bm_free((gattMsg_t *)¬i, ATT_HANDLE_VALUE_NOTI);
}
if does not come back from the GATT_Notification function. During debugging i step in to it GATT_Notification. The program get stuck in section as shown below in figure:
The debugging log show the following at messages:
Tue Oct 24, 2017 11:49:43: The stack pointer for stack 'CSTACK' (currently 0x20001DB8) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:49: The stack pointer for stack 'CSTACK' (currently 0x20001D98) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:51: The stack pointer for stack 'CSTACK' (currently 0x20001D98) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:51: The stack pointer for stack 'CSTACK' (currently 0x20001D98) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:52: The stack pointer for stack 'CSTACK' (currently 0x20001D98) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:54: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:54: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:55: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:56: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:49:57: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
Tue Oct 24, 2017 11:50:03: The stack pointer for stack 'CSTACK' (currently 0x20001D90) is outside the stack range (0x20003B70 to 0x20003F70)
It means that stack is not big enough. Am i right? or is there any other issue?
How i will come to know about the stack memory required by the task ?
I am using the simple_peripheral with
#define SBP_TASK_STACK_SIZE 644
How much maximum stack size i can allocate to a task?
Please help me to figure it out.
I will be waiting for your kind help.
Regards
MAbbas