Tool/software: TI C/C++ Compiler
Hi,
Attached the datasheet of the LCD and the driver code developed using the timer of CC2650.
But there is something which I am missing, but don't know what?
If I am trying to set one segment, let's say just show 1 but it doesn't happen so. Apart from it more segments showed up.
#include "LCD_Driver.h"
#include "stdio.h"
#include "stdint.h"
#include <ti/drivers/PIN.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/drivers/pin/PINCC26XX.h>
#include "GPTimerCC26XX.h"
#include <driverlib/ioc.h>
/*******************************************************************************
********************************************************************************
* Private Definitions
********************************************************************************
*******************************************************************************/
GPTimerCC26XX_Params timerParams;
GPTimerCC26XX_Handle hTimer;
/*******************************************************************************
* General LCD definitions
*******************************************************************************/
#define LCD_REFRESH_FREQ_HZ 30
#define BP_TOTAL 4 // BACK PlANES (COM signals)
#define FP_TOTAL 10 // FRONT PLANES (LCD signals)
// Note: our LCD is spec'd for 3V operation, however, we power the board at
// 3.25V. We compensate for this by inserting a contrast adjustment cycle.
// After stepping through the 4 backplanes we insert one interval (of the same
// length) where all segments are set to 0V. That is, we drive the LCD at 80%
// duty cycle. The RMS voltages scale with the square root of the duty cycle,
// i.e., with sqrt(0.8) ~ 0.89. Our effective drive voltage then becomes
// 3.25 * 0.89 ~ 2.9V. This is suitable for the 3V display and should eliminate
// any ghosting.
/*******************************************************************************
* Timer definitions
*******************************************************************************/
#define gLCDTimer_c gTmr2_c
// We have a 24MHz clock with a 64 prescaler giving a timer clock of 375kHz.
// Devide that by the LCD refresh frequency to get the counter value for one
// full refresh cycle. Within the cycle, however, we need two polarities and
// run through all backplanes plus one contrast adjustment cycle. Hence the
// compare value is
#define gComp1Val_c (375000/(LCD_REFRESH_FREQ_HZ*2*(BP_TOTAL+1)))
/*******************************************************************************
* LCD GPIO assignments
*******************************************************************************/
//static PIN_Handle hLcdPin = NULL;
typedef enum // Port 1 GPIO register bit mapping (back planes)
{
BP0 = GPIO_DIO_22_MASK, //((uint32_t)(1 << 1)), // COM1: GPIO 33
BP1 = GPIO_DIO_21_MASK, //((uint32_t)(1 << 2)), // COM2: GPIO 34
BP2 = GPIO_DIO_20_MASK, //((uint32_t)(1 << 3)), // COM3: GPIO 35
BP3 = GPIO_DIO_19_MASK //((uint32_t)(1 << 4)) // COM4: GPIO 36
}
BP_t;
typedef enum // Port 0 GPIO register bit mapping (front planes)
{
FP0 = GPIO_DIO_18_MASK,
FP1 = GPIO_DIO_17_MASK,
FP2 = GPIO_DIO_15_MASK,
FP3 = GPIO_DIO_14_MASK,
FP4 = GPIO_DIO_13_MASK,
FP5 = GPIO_DIO_12_MASK,
FP6 = GPIO_DIO_11_MASK,
FP7 = GPIO_DIO_10_MASK,
FP8 = GPIO_DIO_9_MASK,
FP9 = GPIO_DIO_8_MASK
}
FP_t;
#define BP_MASK (BP0|BP1|BP2|BP3)
#define FP_MASK (FP0|FP1|FP2|FP3|FP4|FP5|FP6|FP7|FP8|FP9)
#define BP_DATA_SET_REG //GPIO_REGS_P->DataSetHi // BP GPIO registers
#define BP_DATA_RESET_REG //GPIO_REGS_P->DataResetHi
#define BP_DIR_SET_REG //GPIO_REGS_P->DirSetHi
#define BP_DIR_RESET_REG //GPIO_REGS_P->DirResetHi
#define FP_DATA_SET_REG //GPIO_REGS_P->DataSetLo // FP GPIO registers
#define FP_DATA_RESET_REG //GPIO_REGS_P->DataResetLo
#define FP_DIR_SET_REG //GPIO_REGS_P->DirSetLo
#define FP_DIR_RESET_REG //GPIO_REGS_P->DirResetLo
#define BP_RESET_ALL(x) GPIO_setMultiDio(x)
#define BP_SET_REG(x,y) GPIO_writeMultiDio(x,y)
#define BP_RESET_REG(x,y) GPIO_writeMultiDio(x,y)
#define FP_SET_GPIO(x,y) GPIO_writeMultiDio(x,y)
#define FP_RESET_GPIO(x,y) GPIO_writeMultiDio(x,y)
/*******************************************************************************
* 7-Segment digit breakdown
*******************************************************************************/
// Digits on the display are wired into adjacent front planes and accross the
// four back planes. The following define the first front plane for each digit.
#define gLg10_c 0 // Large number tens digit
#define gLg01_c 2 // Large number ones digit
#define gSm10_c 4 // Small number tens digit
#define gSm01_c 6 // Small number ones digit
// We map the 7 segments into a byte where bits from the LSB to the MSB are
// associated with the (back plane, front plane offset) values (0,0), (1,0),
// (2,0), (3,0), (0,1), (1,1), (2,1), (3,1), respectively.
typedef enum
{
SS_F = (1<<0),
SS_G = (1<<1),
SS_E = (1<<2),
// This bit does not coorspond with the 7 segment digit
SS_A = (1<<4),
SS_B = (1<<5),
SS_C = (1<<6),
SS_D = (1<<7)
}
SevenSegMap_t;
// 7 segment digits from 0, ..., 9 are tabulated below. We define the
// additional blank character and the minus symbol at the end of the table,
// with indices
#define gBlank_c 10
#define gMinus_c 11
/*******************************************************************************
********************************************************************************
* Private memory declarations
********************************************************************************
*******************************************************************************/
// Steps within a refresh cycle [+/-]: BP0 BP1 BP2 BP3 CONTRAST
static uint32_t FpOutputs[BP_TOTAL+1] = {0, 0, 0, 0, 0};
static uint32_t BpOutputs[BP_TOTAL+1] = {BP0, BP1, BP2, BP3, BP_MASK};
// Front planes by index
const uint32_t FP[FP_TOTAL] = {FP0, FP1, FP2, FP3, FP4, FP5, FP6, FP7, FP8, FP9};
// Seven segment digit table (0, 1, ..., 9 digits, ' ' and '-')
const uint8_t SevenSegTbl[12] =
{
SS_A|SS_B|SS_C|SS_D|SS_E|SS_F,
SS_B|SS_C,
SS_A|SS_B|SS_G|SS_E|SS_D,
SS_A|SS_B|SS_C|SS_D|SS_G,
SS_B|SS_C|SS_F|SS_G,
SS_A|SS_C|SS_D|SS_F|SS_G,
SS_A|SS_C|SS_D|SS_E|SS_F|SS_G,
SS_A|SS_B|SS_C|SS_F,
SS_A|SS_B|SS_C|SS_D|SS_E|SS_F|SS_G,
SS_A|SS_B|SS_C|SS_F|SS_G,
0x00,
SS_D
};
/*******************************************************************************
********************************************************************************
* Private Prototypes
********************************************************************************
*******************************************************************************/
void LCD_refresh(void);
void LCD_Digit(uint8_t fp, uint8_t digit);
/*******************************************************************************
********************************************************************************
* Public Functions
********************************************************************************
*******************************************************************************/
/*******************************************************************************
* Initialize the LCD driver
*******************************************************************************/
void LCD_Init(void)
{
uint32_t load_value = 799999; // 33 ms
GPTimerCC26XX_Params_init(&timerParams);
timerParams.mode = GPT_MODE_PERIODIC_UP;
timerParams.width = GPT_CONFIG_16BIT;;
hTimer = GPTimerCC26XX_open(GPTIMER0B, &timerParams);
if(hTimer == NULL)
{
Task_exit();
}
// Set timer counting period, 1 tick =1/24000000 second
// Timer starts to count at 0, and the interrupt happens when it wraps around
// so if you want 1 second period, you need to have (24000000 - 1) ticks
GPTimerCC26XX_setLoadValue(hTimer,load_value);
GPTimerCC26XX_registerInterrupt(hTimer, timerCallback, GPT_INT_TIMEOUT);
}
/*******************************************************************************
* Call-back function to refresh the LCD Display at 30Hz
*******************************************************************************/
void timerCallback(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask)
{
LCD_refresh();
}
/*******************************************************************************
* Turn on the display timer - callback will drive LCD
*******************************************************************************/
void LCD_On(void)
{
LCD_Init();
// Enable LCD timer
GPTimerCC26XX_start(hTimer);
}
/*******************************************************************************
* Shut down the display timer and drive all display pins low
*******************************************************************************/
void LCD_Off(void)
{
// Disconnect timer clock source (-> stop)
GPTimerCC26XX_stop(hTimer);
// Turn LCD timer off
GPTimerCC26XX_close(hTimer);
// Drive all LCD GPIOs low
GPIO_clearMultiDio(FP_MASK);
GPIO_clearMultiDio(BP_MASK);
}
/*******************************************************************************
* Set all segments
*******************************************************************************/
void LCD_SetAll(void)
{
uint8_t i;
for(i=0; i<BP_TOTAL; i++)
{
FpOutputs[i] = FP_MASK;
}
}
/*******************************************************************************
* Clear all segments
*******************************************************************************/
void LCD_ClrAll(void)
{
uint8_t i;
for(i=0; i<BP_TOTAL; i++) FpOutputs[i] = 0;
}
/*******************************************************************************
* Set a particular segment
*******************************************************************************/
void LCD_SetSeg(uint8_t fp,uint8_t bp)
{
if(fp < FP_TOTAL && bp < BP_TOTAL) FpOutputs[bp] |= FP[fp];
}
/*******************************************************************************
* Clear a particular segment
*******************************************************************************/
void LCD_ClrSeg(uint8_t fp,uint8_t bp)
{
if(fp < FP_TOTAL && bp < BP_TOTAL) FpOutputs[bp] &= (~FP[fp])&FP_MASK;
}
/*******************************************************************************
* Put number num on the large number display
*******************************************************************************/
void LCD_SetLargeNumber(uint8_t num)
{
// Limit range
if(num>199) num=199;
// First digit (ones)
LCD_Digit(gLg01_c, num%10);
// Decimal right shift
num /= 10;
// Second digit (tens, suppress leading zero)
if(num > 0) LCD_Digit(gLg10_c, num%10);
else LCD_Digit(gLg10_c, gBlank_c);
// Decimal right shift
num /= 10;
// Third digit (hundreds)
if(num > 0) LCD_SetSeg(0,3);
else LCD_ClrSeg(0,3);
}
/*******************************************************************************
* Clear the large number display
*******************************************************************************/
void LCD_ClrLargeNumber(void)
{
LCD_ClrSeg(0,3);
LCD_Digit(gLg10_c, gMinus_c);
LCD_Digit(gLg01_c, gMinus_c);
}
/*******************************************************************************
* Put number num on the small number display
*******************************************************************************/
void LCD_SetSmallNumber(uint8_t num)
{
// Limit range
if(num>99) num=99;
// First digit (ones)
LCD_Digit(gSm01_c, num%10);
// Decimal right shift
num /= 10;
// Second digit (tens, suppress leading zero)
if(num > 0) LCD_Digit(gSm10_c, num%10);
else LCD_Digit(gSm10_c, gBlank_c);
}
/*******************************************************************************
* Clear the small number display
*******************************************************************************/
void LCD_ClrSmallNumber(void)
{
LCD_Digit(gSm10_c, gBlank_c);
LCD_Digit(gSm01_c, gBlank_c);
}
/*******************************************************************************
********************************************************************************
* Private Functions
********************************************************************************
*******************************************************************************/
/*******************************************************************************
* Timer interrupt service routine to drive the display
*******************************************************************************/
void LCD_refresh(void)
{
static uint8_t PLUS = TRUE;
static uint8_t i = 0;
// All BPs inputs (1/2 Vcc)
// BP_RESET_ALL(BP_MASK);
GPIO_clearMultiDio(FP_MASK);
GPIO_setMultiDio(BP_MASK);
if(PLUS)
{
GPIO_setMultiDio(FpOutputs[i]);
GPIO_clearMultiDio(~FpOutputs[i]&FP_MASK);
GPIO_clearMultiDio(BpOutputs[i]);
}
// Negative cycle
else
{
GPIO_clearMultiDio(FpOutputs[i]);
GPIO_setMultiDio(~FpOutputs[i]&FP_MASK);
GPIO_setMultiDio(BpOutputs[i]);
}
// Next plane or ...
if(++i == BP_TOTAL + 1)
{
// ... start over and flip sign
i=0; PLUS = !PLUS;
}
}
/*******************************************************************************
* Encode the 7-segment digit value onto a diplay digit identified by fp.
*******************************************************************************/
void LCD_Digit(uint8_t fp,uint8_t digit)
{
uint8_t i = 0;
// Bitmask for digit value
digit = SevenSegTbl[digit];
// Loop through bits
while(i<8)
{
// Ignore non-7-segment bit 3
if(i!=3)
{
// Set/clear 7-segment element
if(digit&0x01) LCD_SetSeg(fp + i/4, i%4);
else LCD_ClrSeg(fp + i/4, i%4);
}
// Move on
digit>>=1;
i++;
}
}