This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: Example code in ZS-040 (Module use CC2541)

Part Number: CC2541
Other Parts Discussed in Thread: TIDC-SPPBLE-SW-RD, CC2640R2F

Dear all,

Requirement -  IS TO TAKE UART DATA AND TRANSFER THROUGH BLE. I WANT TO TRANSFER AT LEAST 20 FRAMES WHICH INCLUDE 222 BYTES (APPROXIMATELY - 4500 BYTES PER SECOND).

I cannot achieve this requirement using ZS-040 module (Which has CC2541). But the code in the module is exact what I required. [Which has only one service - one characteristic with read & write the data to UART]. I want this code so I can use it in CC2640R2 LP. I can have a stable transferring through UART to BLE.

Kind regards

Dulip