Part Number: CC256XMS432BTBLESW
Other Parts Discussed in Thread: CC2564C
We build the "SPPLEDemo", but the binary size comes to 255KB (MSP432 is 256 KB). We need to add some more functionalities to the application but since the image is this big, it is not possible.
The option to configure (add or remove BT components) should be available in FBL build script "fbl_gen.pl" as per TI documents.
Also please let us know if we are doing anything wrong during build as the size seems too big.
But this file is missing in my installation directory. Could you please provide this script "fbl_gen.pl" as we need to reduce the memory size.
Library Used : Bluetopia_Full.lib
ROM Used : 0x0003fee4 (bytes)
RAM Used : 0x0000792c (bytes)