This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Hi,
I am trying to use periodic interrupts to generate a signal at set intervals. The periodic interrupts work, but when I try to communicate with an external DAC to generate the signal I run into some problems. I have written a function to send a specified voltage to the DAC, but it doesn't work properly when called from the ISR. I had a look at the signals on a scope and noticed that the i2c communication is much shorter (~150 uS) when the function is called from the ISR compared to when it is run from the main function (~400 uS). Can someone explain to me why this happens and how I can fix it?
Kind regards,
Lukas
Hi,
Thanks for your reply. I also thought that the RTOS might be cutting off the I2C communication, so I had a closer look at the scope traces. When calling my function from the main loop, I get the expected communication:
0x98 (addr. is 0x4C + write bit), 0, (ack), 0x10 (control byte), 0 (ack), 0x7F (frist data byte), 0 (ack), 0xFF (second data byte), 0 (ack).
However, when calling my function from an ISR, it is not a truncated version of that communication but something seemingly random. From my observations, one of 2 things occurs. Either:
0x22 (addr would be 0x21 + write bit), ack, 001 (binary)
and then cut off, or:
0x21 (addr woul be 0x20 + read bit) and then the clock line stays low for what would be another 4 pulses before going back high.
So clearly the I2C line isn't just being cut off, it is just transmitting nonsense. Can you think of a reason this might happen in an ISR but not in the main loop? Can the I2C bus just not be used inside an ISR?
Kind regards,
Lukas
Update:
I was using the I2C in blocking mode, and blocking functions are not allowed during interrupts which caused the problem. I still don't understand why the first few bits were sent, but when using callback mode it works. However, there are problems if the I2C transaction doesn't finish before the ISR (because in my case the I2C_Handle and I2C_Transaction are local variables to the ISR).