Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640,
I'm using the CC2640R2F for a new design. I've used the Sensor Controller before (on another design using CC2640), but want to use it in a different mode this time.
I'm confused with the documentation on the Execution modes. I understand the concept of Init, Execution, Event handling, termination. In my previous project I just used the Execution mode, putting the code into a loop that did the appropriate things. For this project, I'd like to initialize some things (including a timer), then collect data each time the timer fires.
The documentation implies that the timer only runs using the 32 KHz clock, but other documentation (Peripherals->Timer 0) allows periodic events at uSec resolutions. Is there a way to trigger the Event Code using Timer 0 (so the Event code can be called every ~700 uSec)? Or are the calls related to Timer 0 only available inside task code (eg. can't be used to initiate a task block)?
Thanks!