This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi!
In order to test a setting of the power control of the CC2640, we would like to generate a new CC26xx.bin file in the blefi project. I have tried to follow the instructions given in tidua62b, but I guess the SDK and the CC has changed a bit since this document was written. Using the CCS I have imported the host_test projects for both lp and em, but from the Board files I see there is no match in the pin configuration compared to the schematic tidrgi8a.pdf. I could modify these to match the schematic, but there some signals that I can't sort out. For example the interchip and hs lines. I am thus wondering if the source code for this project is available? If not, can I use the standard host_test code under the lp or em project along with a modified board file?
Best regards,
Jan