This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640R2F: Hard Reset after Programming

Part Number: CC2640R2F

Tool/software: TI-RTOS

Is it compulsory to give hard reset after burning the hex file? Is there any setting in which we dont need to give hard Reset after programming?


Thanks

  • Hi Sumair,

    Can you clarify what you mean by a hard reset? Is there a reason you do not want to perform a reset?
  • Hard Reset means to unplug the power source.

    "I am using "HAL_SYSTEM_RESET();" whenever I will receive reset command from UART.
    But it fails every time after using JTAG (programming with CCS, also with Flash Programmer 2).
    However, it work fine when i power off and on the board after JTAG programming."

    The difference is that I am using XDS100 Ver3.0, XDS-FTZ5PP2UA instead of XDS110

    I have also replaced xds drivers inside <fp2_install_dir>/config/xds/*, but the problem is still not reloved

    I also used UniFlash to program the circuit but result is still same.