This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2650: from where i can find Bluetooth developer studio (BDS) plugin for CC2650

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, CC2640R2F, SIMPLELINK-CC2640R2-SDK

(Mod edited for correctness)

Tool/software: Code Composer Studio

from where i can download the Bluetooth Development studio plugin for CC2650.

   on this website the BDS plugin is available for CC2640R2F not for CC2650. please help me regarding this issue i am trying to create the profile for Bluetooth (CC2650 launchpad) but i got error.

Edited

  • please reply me soon whether BDS plugin for cc2650 is available or not. i am waiting for the answer
  • Hello Pradeep,

    The BDS plugin is only available for the SIMPLELINK-CC2640R2-SDK. We do recommend that you start new BLE-only designs with the CC2640R2F.

    Best wishes
  • ok thanks for the reply. i just want ask you one thing. i am going to use CC2650 for developing motion tracking device for sports like Golf, so in golf i am going to track the position and velocity of Club and hand, swing plane and for calculating the distance of ball in yards. so i will interface IMU, Display and the GPS with the CC2650. so the question is , is it good to choose the CC2650 for this purpose, and does the well resource available for programming using CC2650 because i did not find any tutorials other than Texas instruments Resource Explorer, and the Texas documentation is only based on defined example means this documentation does not tell about the programming, interfacing of LCD, IMU and coding. so i have doubt whether i should use CC2650 or not because the project is going to be complex and the programming of CC2650 is also typical. I am new to this Platform please guide me regarding this issue.