Hi all,
Application we are developing is time sensitive and we are looking for ways to control the wireless transmission delay. In ideal case, when a packet (notification) is not sent within certain timeframe we would like to be able to discard it (as it is not useful for receiver app) and try to transmit the next packet in line. By doing so we would stay within the delay budget with the transmission (but purposely loosing/dropping packets as a trade-off).
The problem is that, and correct me if I am wrong, once a packet is forwarded to the BLE stack for a transmission (by issuing GATT_notification command) there is very little control over what can happen to it. BLE stack will try to retransmit that particular packet until supervision timeout is reached, however in this case not only that the active packet is dropped but so it the BLE connection it self. This is a bit of suboptimal scenario.
Is there a way around it? Is it possible to stop BLE retransmission after a certain amount of time and give it a new packet/value to transmit, but then drop the connection only if such a scenario repeats for defined amount of times?
Cheers,
Nenad