Part Number: CC2564MODN
Team,
We uses the CC2564MODN+MK22FN1M0AVMC12 suffers from a strange behavior of Bluetopia.
Our Apps based on SPPDemo does not detect the linkloss between the
remote device sometimes.
Customer also took a look into the BT Log via the debug port using the logger.
The BT Log tells the CC2564MODN certainly outputs
"HCI_Disconnect_Complete_Event" with reason code "Connection
Timeout(=0x08)".
However, the Bluetopia has never informed the disconnection of the link to Apps.
Also look into the UART driver. The last Rx Data from the CC2564MODN
would be "04:05:04:00:01:00:08",
matching "HCI_DISCONNECTION_COMP_EVT".
Could you please let me know how to solve it?