Part Number: CC2640R2F
Dear TI Community,
We are using two CC2640R2 launchpad boards to evaluate Bluetooth Low Energy long range functionality. So far we have tried communication between two boards with 2 examples from Github - longrange (central + peripheral) and throughput (central + peripheral).
We have not managed to establish a long range connection (maximum about 10 meters, or less), despite adding a little antenna on the peripheral board. My question is, is there some setting I need to modify in the code or in the menus when using the examples?
And also, when it comes to long range functionality, how is longrange demo different from throughput demo? I see that both of the demos support S8 encoding, with no other major difference at first sight.
Thank you very much and best regards!
J Crater