Other Parts Discussed in Thread: CC2540,
Tool/software: Code Composer Studio
Sir,
I want to make a project using CC2650 Launchpad that can scan all the nearest bluetooth devices as well as can advertise by which all the nearest devices can connect with CC2650 Launchpad. I am going to use CC2540 and CC2650 launchpad. when CC2650 scan the nearest device so it can scan the CC2540 and connect with the CC540 using bluetooth. When CC2650 advertise then an android phone can detect and connect with CC2650 so i can transfer all the sensor Data from CC2650 to Android phone. i have seen the project zero and it is working properly but i am not able find how the programming for Bluetooth communication is done so it can advertise and receive/send the Data in Project zero. I want to scan the nearest devices and want to send the character and integer data. Can anyone guide how i can do this what are steps i need to to or is there any tutorial available. i want to this from scratch
Thank you