Tool/software: TI-RTOS
Hello,
I am working on LaunchXL-CC2640R2F, i want to interface an accelerometer which is an I2C based sensor, i have referred I2C driver Example from CC2640R2 SDK, using the designated pins( DIO4 and DIO5) referred in the I2C driver example i am getting response from the sensor, but i wanted to use DIO2 and DIO3 for same sensor,
I made the respective changes in CC2640R2_LAUNCHXL.h file, however i am not getting any response from the sensor,
The similar way i tried on CC2650-LaunchXL but i am facing the same issue,
So i checked the pin status by connecting LED on that pin, i can see that it is remaining high all the time,
Please let me know is there any required change to be made so that i can use these pin (DIO2 and DIO3) for I2C and also let me if there any other pins i can use for I2C interface except (DIO4 and DIO5)