This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540: Trying to connect CC2540 with Com port.

Part Number: CC2540
Other Parts Discussed in Thread: CC2540

Hello everyone

I have successfully programmed the HostTest.hex file to the IC. I am know trying to connect it to my Laptop with Bluetooth but my laptop wont connect to it. I see a ble device that has as name Unknown and i am almost 100% sure this is my cc2540. But when i click pair it says: "try again and make sure your device is still discover able". I have done a verify against the HostTest hex file and gives OK. So firmware must be correct. The cc2540 is now still connected to the cc debugger for power. 

The CC2540 is on a small circuit board and it worked before in bleutooth peripheral mode. 

Laptop = windows 10

Greetings Sieuwe