Part Number: CC2640
Other Parts Discussed in Thread: BLE-STACK, , , CC2650
Tool/software: TI C/C++ Compiler
Hello, I can't seem to build even a skeleton CC2640F128 project.
* I have built the simple_peripheral_cc2640r2lp_app project and successfully run it on the eval board.
* I could not port it to the F128 (our target) by just switching the CPU, however.
* I tried building a skeleton project - but it fails due to what looks like missing reset code.
* So far I haven't found any refs to the "ResetISR" (see below) code anywhere in the docs.
* Shouldn't a skeleton build without modification?
SKELETON PROJECT CREATION
-----------------------------
New CCS Project
Target: SimpleLink Wireless MCU CC2640F128
Connection: TI XDS2xx USB Debug Probe
Project Name: Test_CC2640F128
Use Default Location: Checked
Compiler Version: TI v 16.9.6.LTS
(No advanced settings modified)
Project Template: Empty Project (with main.c)
BUILD RESULTS
------------------------
'Building target: Test_CC2640F128.out'
'Invoking: ARM Linker'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7M3 --code_state=16 -me -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi -z -m"Test_CC2640F128.map" --heap_size=0 --stack_size=256 -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="Test_CC2640F128_linkInfo.xml" --rom_model -o "Test_CC2640F128.out" "./main.obj" "../cc26x0f128.cmd" -llibc.a
<Linking>
undefined first referenced
symbol in file
--------- ----------------
ResetISR
error #10234-D: unresolved symbols remain
warning #10062-D: entry-point symbol "ResetISR" undefined
error #10010: errors encountered during linking; "Test_CC2640F128.out" not built
>> Compilation failure
makefile:141: recipe for target 'Test_CC2640F128.out' failed
makefile:137: recipe for target 'all' failed
gmake[1]: *** [Test_CC2640F128.out] Error 1
gmake: *** [all] Error 2
**** Build Finished ****
------------------------------------------------------------------------------