This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Simultaneous 802.15.4 and BLE

Part Number: CC2650
Other Parts Discussed in Thread: CC1350,

Hello,

Is it possible to run a BLE connection to a phone, and a separate mesh connection (over either BLE5 or 802.15.4-related stack) using the CC2650?  Or even the CC1350 on Sub-Ghz if possible.  We have chosen no stack or standard; the only thing that is necessary is a BLE connection (as peripheral) and a Mesh connection (collecting data from multiple nodes).

  • Sorry actually let me correct that in the above:

    >> ...and a Mesh connection (collecting data from multiple nodes).

    it is not only collecting data from nodes, we would also be transmitting data to nodes as well.
  • Hello,

    Concurrent protocol support is not available on the CC26x0 or CC13x0 devices; however, this is a feature targeted for CC26x2. Please register for updates on the SIMPLELINK-CC26X2-SDK & SIMPLELINK-CC13X2-SDK pages with the "Alert Me" button so you are notified when the SDK is available shortly.

    Best wishes