Part Number: CC256XM4BTBLESW
I work with the SPPDemo.
I send to SPPDemo:
client
Inquiry
pair 1 1
open 1 1
Then the port open needs 100 ms to connect.
When I reset the device, and send
Inquiry
open 1 1
the Open needs 3000 ms
The System have Lost the pairing.
What can I do to hold the pairing after reset?
I write back the KeyLink from
I write back the LinkKeyInfo with LinkKey Values what I get from atLinkKeyCreation after pairing bevore reset.
But SPP_Open_Remote_Port does not use LinkKeyInfo.
And I get no Authentication callback from remote device after SPP_Open_Remote_Port.
This is the reason I can not send GAP_Authentication_Response with the LinkKeyInfo to the Device.
What we need is, the same speed for SPP_Open_Remote_Port then bevore Reset.
I dont want send an pairing after reset because it is too slow.