Part Number: CC2540
Hi,
I am interested to find out about the my CC2540 ADC conversion power consumption.
First allow me to describe my set up.
(1) below is the code i use. P06 detect ADC input and measure with resolution 8. It will sample ADC value of P06 in an event every 1 sec.
(2) I measure with similar set up as described in AN09 power consumption measurement set up.
http://www.ti.com/lit/an/swra347a/swra347a.pdf
Put 10 ohm resistor in front and measure the voltage across that 10 ohm with oscilloscope.
Then measure duration and current level during an event and put those info inside the power consumption excel file as below:
www.ti.com/.../litabsmultiplefilelist.tsp
I get my results to be 35 micro Amp during that event that has ADC sampling.
My Questions are as follows:
(Q1) From following document from TI "http://www.ti.com/lit/ds/swrs084f/swrs084f.pdf"it shows that ADC consumption is significantly high than mine. So my method is measuring ADC consumption is not correct?
(Q2) If my measurement method is not correct, then can anyone kindly suggest the appropriate method for such measurement?
P.S The reason I want to verify is because, in my implementation, I am going to run some algorithm based on ADC value during that event. And I wants to find out the consumption of that whole event, which involve both ADC conversion/ ADC value detection + algorithm. In above code, i did not show that algorithm.
Regards,
LB