Part Number: CC2640R2F
Hello,
We want to use the cc2640r2f as a BLE network controller for BLE 5 long range and BLE 4.2 compatibility mode. We had discussed and have got information that there will be memory limitation in terms of using cc2640r2f as a application controller with encryption security. We want to estimate that will it be possible to implement the network controller using BLE 5 long range or not.
we will interface the module with an external MCU which will run the complete end application. On BLE side, we want to do the following tasks:
1) Scan either of the BLE beacons over BLE 4.x or BLE 5 long range as configured
2) Advertize or broadcast the BL beacons over BLE 4.x or BLE 5 as per requirement
3) Form a connection with other device as a slave (one device at a time) over BLE 4.x or BLE 5 long range.
We can work on using the HCI command sort of interface which can be run on our host MCU and cc2640r2f need to have the complete stack for BLE 5 long range and BLE 4.x backward compatibility.
Please suggest if there is any application which can be referred to do a demo for this application?
Regards
Prateek