Hi, TI engineers,
I have encountered a tough issue. Two paired CC2540 devices that central and peripheral device, without any operation action only at the paired status , had an abnormal disconnection, and the central device didn't receive any terminate event.
I modified the supervision timeout setting, TGAP_CONN_EST_SUPERV_TIMEOUT, changing to 200 value, at the initial of the simpleBLEState on the central device.
I don't know whether the issue is caused by the error supervision timeout setting.
Could TI engineers help to answer the question?
Thank you.
SunnyHua