This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Load Impedance Mismatch

Part Number: CC2640R2F

How much is the CC2640R2F efficiency affected by the load impedance missmatch?

To be specific, customer has an antenna with Return Loss around 7 dB (Antenna Impedance as measured by the Network Analyzer: 21 – j6 Ohms). I understand that the CC2640R2F amplifiers are going to have their efficiency dropped due to the loading, Probably, the effect is not symmetric, as the receiver LNA is a different class than the transmitter power amplifier.

My question: The RL of the antenna causes transmit power loss around 1 dB, and assuming 2 dB loss on the RF path and Balun, as the total radiated power of the system is around – 7 dBm, is it possible that the missmatch is causing the 4 dB drop?

Thanks,
Mark

  • Hi Mark,

    The datasheet numbers for the CC2640R2F are measured at the antenna feed point on the EVM. If the customer has implemented the balun and RF filter/match as in the reference design, the 7 dB loss is caused by antenna mismatch and efficiency.

    A start here would be to do a conducted measurement at the antenna feed point (with antenna and antenna matching disconnected) to verify the conducted power.

    Regards,
    Fredrik
  • Hi Fredrik,

    The conducted measurements with a UFL cable at the Balun output are good as compared to the selected output power of the CC2640R2F. Thus, we conclude that the antenna miss-match loss and efficiency has dropped due to the load impedance. Would you agree?

    Thanks for the support.

    Regards,
    Mark
  • Hi Mark,

    Yes, it sounds like the antenna mismatch causes the drop in TRP.

    Regards,
    Fredrik