Part Number: CC2640R2F-Q1
Other Parts Discussed in Thread: CC2640R2F
Dear Experts,
my customer is using IAR 8.11.2 with BLE stack v1.50.00.58 on custom CC2640R2F board. Their SW is based on our multi_role example with several adaptations and changes.
They are seeing a very strange issue at the moment.
If they use the "Download and Debug" option in IAR and then let the application run --> "Go", everything seems to work fine and they are able to communicate over SPI and also able to see advertising starting and so on ...
If they on the other hand either use FlashProgrammer2 or also IAR to download the application, then do a reset of the board and use it in standalone mode without debugger/emulator connection, the application is not working properly --> SPI communication is not working and thus advertising is not seen. Also if they then connect to the target using "Debug without Downloading" they see, that they are running into ICall timeout everytime.
Any ideas/hints what exactly is going wrong or might be different between "loading and running via emulator" vs. "loading, reset and running standalone or in Debug without Downloading" mode? There must be something set or configured by the emulator in case it is used directly after loading the application image ...
Many thanks and best regards,
RogerG