This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F-Q1: CC2640R2F DTM/PTM support,

Part Number: CC2640R2F-Q1
Other Parts Discussed in Thread: BLE-STACK

Hi,

With regards to configuring CC2640R2F-Q1 to bluetooth DTM/PTM modes
could you please let us know the information for below questions.

1.For DTM we need UART interface whereas PTM supports both UART & SPI?

2.For DTM, is the UART port fixed? or we can use any available UART port?

3.For DTM the ports required are TX/RX and VDD/GND only?

4.For PTM we can choose either SPI/UART and the ports are not fixed?
   and does TI provide sample codes in case of SPI interface?

Best Regards
paddu