Tool/software: TI-RTOS
Hi TI experts,
I found an interesting Current Spike issue on LAUNCHXL-CC2640R2, and below is the steps to reproduce it on LAUNCHXL-CC2640R2.
1. Import the project simple_peripheral_cc2640r2lp_oad_offchip_app to CCS with bim and stack from the latest SDK cc2640r2_sdk_1_50_00_58
2. Apply the diff (add external page erase every 5 min) to simple_peripheral_oad_offchip.c
3. Build and load it to LAUNCHXL-CC2640R2 with a multiple-meter to measure the Current and Voltage
4. After a few hours, I got the Current and Voltage results as showing in the attached picture.
My question is how I can solve the Current Spike issue? Since it will damage the battery and cause cc264or2f reset.
Current spike screenshot,
the diff file added to run external flash page erase every 5 minutes.
diff --git a/simple_peripheral_oad_offchip.c b/simple_peripheral_oad_offchip.c
index de123d0..5cc6a2d 100644
--- a/simple_peripheral_oad_offchip.c
+++ b/simple_peripheral_oad_offchip.c
@@ -651,6 +651,24 @@ static void SimpleBLEPeripheral_init(void)
}
}
+
+#include "flash_interface.h"
+static uint32_t global_timer = 0;
+static uint32_t current_page = 0;
+void current_spike_page_erase(void)
+{
+ if( global_timer % 60 == 0 )
+ {
+ if ( flash_open() )
+ {
+ current_page = current_page % 256;
+ eraseFlash(current_page);
+ current_page ++;
+ }
+ }
+ global_timer ++;
+}
+
/*********************************************************************
* @fn SimpleBLEPeripheral_taskFxn
*
@@ -797,6 +815,7 @@ static void SimpleBLEPeripheral_taskFxn(UArg a0, UArg a1)
if (events & SBP_PERIODIC_EVT)
{
Util_startClock(&periodicClock);
+ current_spike_page_erase();
// Perform periodic application task
SimpleBLEPeripheral_performPeriodicTask();
@@ -1265,7 +1284,7 @@ static void SimpleBLEPeripheral_processStateChangeEvt(gaprole_States_t newState)
break;
case GAPROLE_WAITING:
- Util_stopClock(&periodicClock);
+// Util_stopClock(&periodicClock);
SimpleBLEPeripheral_freeAttRsp(bleNotConnected);
Display_print0(dispHandle, SBP_ROW_CONN_STATUS, 0, "Disconnected");
I know there is a power consumption bible available at
but it doesn't help to resolve the current spike issue.
Thank you,
David