This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: in debugging

Part Number: CC2640

in IAR i am getting this type of error please help me.?

Tue Mar 06, 2018 11:59:49: Fatal error: Failed to connect to the XDS emulator (connect ICEPick)... (Error -233 @ 0x0) The JTAG IR and DR scan-paths cannot circulate bits, they may be broken. An attempt to scan the

JTAG scan-path has failed. The target's JTAG scan-path appears to be broken with a stuck-at-ones or stuck-at-zero fault. (Emulation package 6.0.83.1) Session aborted!

Tue Mar 06, 2018 11:59:49: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3_2\arm\config\flashloader\TexasInstruments\FlashCC26xx.mac