Part Number: CC2541
Hi,
I designed a CC2541 board based on the reference design. I can load firmware to the CC2541 from IAR through CC Debuger, but it does not boradcasting and I could not see it on lightblue. I suspected the crystal and read the thread attached. I found both the resistances between XOSC_Q2 and XOSC_Q1 are 1.7ohm, which means the connection is good. However, when I probing this two pins I can see the very fuzzy output (may be the frequency too high and too much noise), but XOSC_Q2 has a DC voltage of 2V but XOSC_Q1 has almost 0V. Is this normal? What is the expected output of both XOSC_Q1 and XOSC_Q2? what could be the place other to start debugging?
Thank you