This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: Question on HCI xml script (incl. VS commands) for use with CC2640R2 host_test example and HCI Tester

Part Number: LAUNCHXL-CC2640R2


Hi!

I have some basic questions related to CC2640R2 when used with the host_test example in the SDK. Specifically I would like to know:

1. Is there a HCITesterXML file for use with HCITester where the xml supports CC2640R2 (i.e. any VS commands for CC2640R2 etc)?

2. Which version of the HCI Tester is the applicable one to use today, is 3.0.0.37 from 2015 is the relevant version?

3. HCI Tester cannot be used in an automated environment being remote (e.g. executed via command line interface), or?

4. Where can I find useful script files (.bts) for use with HCITester? For example scripts for initializations for central role, peripheral role etc?

5. Are there any other scripts available for use for stability testing (e.g. for use in a automated test environment)?

6. How about support for Python, are there any scripts for HCI if using CC2640R2 (here I assume a setup based on python for automation)?

Thanks in advance.

BR, Patrik