Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Board: cc26xr1 (cc2652r1f uC)
CCS: v7
I'm am trying to run the ProjectZero example with the newly acquired cc26xr1 but after have flashed the board (debugging) and hitting play, I get the following error:
- Cortex_M4_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0)
- Cortex_M4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
I have reseted the board, erased the entire flash (with uniflash), updated the xds110 firmware and changed the optimization levels to 0.
What do I do to run this simple example?