This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: Project

Part Number: CC2650STK

Hi,

I have got a cc2650STK sensortag.

I am trying to develop the sensor in such a way that it can retrieve and send data to another sensor.

Which means it is also need a direct connection to another sensor.

My first question is " IS THIS THING EVEN POSSIBLE? IF YES, HOW CAN I DO IT?"

Secondly, what I am trying is,  to use ble_sdk--> examples, open them in Code composer and build and debug them. 

After all this is done i am converting it to hex file and combine it with simple_peripheral.hex file and flash it to sensor using flash programmer.

Am i doing it correctly? Will it work? If any, suggestions please tell me and help me get this done. 

Thank you

Regards

Rishabh Jain 

rishabhj14@yahoo.com