This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/CC2640: CC2640 OAD Development using custom PCB as downloader with the help of XDS100V3

Part Number: CC2640
Other Parts Discussed in Thread: CC2650, , CC2540

Tool/software: WEBENCH® Design Tools

My CC2650 Launchpad got damaged due to some short circuit.

I am developing OAD on cc2640 device.

I have downloaded combined target code(unified hex file) on one of the CC2640 custom device device.

now i want to setup the host.Can I use my cc2640 PCB as host and download code into CUSTOM TARGET BOARD through BTOOL using xds100v3.

In short can i use my custom board as downloader with the help of xds100v3 debugger?

How BTOOL communicate with launchpad? JTAG or UART?

My challenge is developing CC2640 OAD using two cc2640 custom PCB and XDS100V3 Debugger.

did anyone else tried this?