Part Number: CC2540
Hi Team,
I have been searching e2e posts for corrupt UART data; most posts seem to address Tx side while my issue is with Rx side on CC2540 (external Tx side pretty well tested and flushed out).
I found this e2e post which essentially suggests that if you are using UART w/ DMA, you should ensure the HCI_EXT_ClkDivOnHaltCmd() function is not called; even though not using DMA I tried this but no luck.
two questions:
1) Any idea what can be causing me to receive garbage data in ~5% of my messages?
2) when it comes to commenting out HCI_EXT_ClkDivOnHaltCmd() function, I see the comments suggests MCU is halted when network processor is active; is this true and could this be contrinuting to the issue I am seeing?
// Enable clock divide on halt
// This reduces active current while radio is active and CC254x MCU
// is halted
// HCI_EXT_ClkDivOnHaltCmd( HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT );