Part Number: CC2650
Other Parts Discussed in Thread: CC3200
Tool/software: Linux
Hello everyone,
I have bought TI CC2650 LaunchPad, but faced with issue. This board is not recognized by Ubuntu 16.04. On Windows platform all work properly. Board is recognized and I can even debug some software on it. It is an issue only on LInux
Another my board TI CC3200 is recognized by Ubuntu, I guess because there are used FTDI chip and it is recognized as /dev/ttyUSB1
In CCS Studio an issue gotten:
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ /home/redra/.ti/ti/2/0/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'libjioxds110.so'. The library build date was 'Feb 8 2018'. The library build time was '18:25:14'. The library package version is '7.0.188.0'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-260' (0xfffffefc). The title is 'SC_ERR_XDS110_OPEN'. The explanation is: An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. [End]
Had anyone such kind of issues ?