This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640R2F: Custom designed board CC2640R2F board lock

Part Number: CC2640R2F


Tool/software: TI-RTOS

i have designed custom board using CC2640R2F chip for project,

We have development application code on CC2640R2F_LAUNCHXL it's working fine. 

 But in our final device design we used "(5-mm × 5-mm RHB VQFN32 (15 GPIOs) "chip while debugging we have changed board file according to CC2640R2DK_5XD .c and .h file (which is imported form the path "C:\ti\simplelink_cc2640r2_sdk_1_50_00_58\source\ti\blestack\boards\CC2640R2DK_5XD")

where we found i2c is not initialized, as my project includes i2c we referred i2c initialization of CC2640R2F_LAUNCHXL  and did the changes in board and CC2640R2DK_5XD  files  which i have attached below.

Pins used are I2C_SCL as IDIO4 and I2C_SDA as  IDIO5, 

Now the issue is that whenever run basic code of I2C or our final developed firmware, the custom board getting locked and getting below error 

"IcePick_C: Error connecting to the target: (Error -275 @ 0x0) The attempt to poll a target device exceeded its timeout limit. The utility or debugger has requested that a target device be repeatedly accessed for a specific data or status value. This has failed because the built-in limit for the maximum number of attempts when polling the JTAG scan-path has been exceeded. (Emulation package 7.0.100.0)"

To resolve this issue we have followed the SmartRF Flash programmer 2. "Mass Erase option" but didn't solve my issue. Please let me know the step by step procedure to unlock the board.

Please check the attached files and suggest me if there is any issue in configuration I2C and initializing the other respected pins for project. 

1348.Board.h

/*
 * Copyright (c) 2015-2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */


/*
 *  ====================== CC2640R2DK_5XD.c =====================================
 *  This board file is made for the 5x5 mm QFN package, to convert this board
 *  file to use for other smaller device packages please refer to the table
 *  below which lists the max IOID values supported by each package. All other
 *  unused pins should be set to IOID_UNUSED.
 *
 *  Furthermore the board file is also used
 *  to define a symbol that configures the RF front end and bias.
 *  See the comments below for more information.
 *  For an in depth tutorial on how to create a custom board file, please refer
 *  to the section "Running the SDK on Custom Boards" with in the Software
 *  Developer's Guide.
 *
 *  Refer to the datasheet for all the package options and IO descriptions:
 *  http://www.ti.com/lit/ds/symlink/cc2640r2f.pdf
 *
 *  +-----------------------+------------------+-----------------------+
 *  |     Package Option    |  Total GPIO Pins |   MAX IOID            |
 *  +=======================+==================+=======================+
 *  |     7x7 mm QFN        |     31           |   IOID_30             |
 *  +-----------------------+------------------+-----------------------+
 *  |     5x5 mm QFN        |     15           |   IOID_14             |
 *  +-----------------------+------------------+-----------------------+
 *  |     4x4 mm QFN        |     10           |   IOID_9              |
 *  +-----------------------+------------------+-----------------------+
 *  |     2.7 x 2.7 mm WCSP |     14           |   IOID_13             |
 *  +-----------------------+------------------+-----------------------+
 *  ============================================================================
 */

#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>

#include <ti/devices/cc26x0r2/driverlib/ioc.h>
#include <ti/devices/cc26x0r2/driverlib/udma.h>
#include <ti/devices/cc26x0r2/inc/hw_ints.h>
#include <ti/devices/cc26x0r2/inc/hw_memmap.h>

#include "CC2640R2DK_5XD.h"

/*
 *  =============================== Power ===============================
 */
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>

const PowerCC26XX_Config PowerCC26XX_config = {
    .policyInitFxn      = NULL,
    .policyFxn          = &PowerCC26XX_standbyPolicy,
    .calibrateFxn       = &PowerCC26XX_calibrate,
    .enablePolicy       = TRUE,
    .calibrateRCOSC_LF  = TRUE,
    .calibrateRCOSC_HF  = TRUE,
};

/*
 *  =============================== Crypto ===============================
 */
#include <ti/drivers/crypto/CryptoCC26XX.h>

CryptoCC26XX_Object cryptoCC26XXObjects[CC2640R2DK_5XD_CRYPTOCOUNT];

const CryptoCC26XX_HWAttrs cryptoCC26XXHWAttrs[CC2640R2DK_5XD_CRYPTOCOUNT] = {
    {
        .baseAddr       = CRYPTO_BASE,
        .powerMngrId    = PowerCC26XX_PERIPH_CRYPTO,
        .intNum         = INT_CRYPTO_RESULT_AVAIL_IRQ,
        .intPriority    = ~0,
    }
};

const CryptoCC26XX_Config CryptoCC26XX_config[CC2640R2DK_5XD_CRYPTOCOUNT] = {
    {
         .object  = &cryptoCC26XXObjects[CC2640R2DK_5XD_CRYPTO0],
         .hwAttrs = &cryptoCC26XXHWAttrs[CC2640R2DK_5XD_CRYPTO0]
    },
};

/*
 *  =============================== Display ===============================
 */
#include <ti/display/Display.h>
#include <ti/display/DisplayUart.h>

#ifndef CC2640R2DK_5XD_DISPLAY_UART_STRBUF_SIZE
#define CC2640R2DK_5XD_DISPLAY_UART_STRBUF_SIZE    128
#endif

DisplayUart_Object        displayUartObject;

static char uartStringBuf[CC2640R2DK_5XD_DISPLAY_UART_STRBUF_SIZE];

const DisplayUart_HWAttrs displayUartHWAttrs = {
    .uartIdx      = CC2640R2DK_5XD_UART0,
    .baudRate     = 115200,
    .mutexTimeout = (unsigned int)(-1),
    .strBuf       = uartStringBuf,
    .strBufLen    = CC2640R2DK_5XD_DISPLAY_UART_STRBUF_SIZE,
};

#ifndef BOARD_DISPLAY_USE_UART
#define BOARD_DISPLAY_USE_UART 1
#endif
#ifndef BOARD_DISPLAY_USE_UART_ANSI
#define BOARD_DISPLAY_USE_UART_ANSI 0
#endif

/*
 * This #if/#else is needed to workaround a problem with the
 * IAR compiler. The IAR compiler doesn't like the empty array
 * initialization. (IAR Error[Pe1345])
 */
#if (BOARD_DISPLAY_USE_UART)

const Display_Config Display_config[] = {
#if (BOARD_DISPLAY_USE_UART)
    {
#  if (BOARD_DISPLAY_USE_UART_ANSI)
        .fxnTablePtr = &DisplayUartAnsi_fxnTable,
#  else /* Default to minimal UART with no cursor placement */
        .fxnTablePtr = &DisplayUartMin_fxnTable,
#  endif
        .object      = &displayUartObject,
        .hwAttrs     = &displayUartHWAttrs,
    },
#endif
};

const uint_least8_t Display_count = sizeof(Display_config) / sizeof(Display_Config);

#else

const Display_Config *Display_config = NULL;
const uint_least8_t Display_count = 0;

#endif /* (BOARD_DISPLAY_USE_UART) */

/*
 *  =============================== GPIO ===============================
 */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/gpio/GPIOCC26XX.h>

/*
 * Array of Pin configurations
 * NOTE: The order of the pin configurations must coincide with what was
 *       defined in CC2640R2DK_5XD.h
 * NOTE: Pins not used for interrupts should be placed at the end of the
 *       array. Callback entries can be omitted from callbacks array to
 *       reduce memory usage.
 */
GPIO_PinConfig gpioPinConfigs[CC2640R2DK_5XD_GPIOCOUNT] = {
    /* Input pins */
    GPIOCC26XX_DIO_19 | GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_RISING,  /* Button 0 */
    GPIOCC26XX_DIO_12 | GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_RISING,  /* Button 1 */

    /* Output pins */
    GPIOCC26XX_DIO_25 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,  /* LED1 */
    GPIOCC26XX_DIO_27 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,  /* LED2 */
    GPIOCC26XX_DIO_07 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,  /* LED3 */
    GPIOCC26XX_DIO_06 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,  /* LED4 */
};

/*
 * Array of callback function pointers
 * NOTE: The order of the pin configurations must coincide with what was
 *       defined in CC2640R2DK_5XD.h
 * NOTE: Pins not used for interrupts can be omitted from callbacks array to
 *       reduce memory usage (if placed at end of gpioPinConfigs array).
 */
GPIO_CallbackFxn gpioCallbackFunctions[] = {
    NULL,  /* Button 0 */
    NULL,  /* Button 1 */
};

const GPIOCC26XX_Config GPIOCC26XX_config = {
    .pinConfigs         = (GPIO_PinConfig *)gpioPinConfigs,
    .callbacks          = (GPIO_CallbackFxn *)gpioCallbackFunctions,
    .numberOfPinConfigs = CC2640R2DK_5XD_GPIOCOUNT,
    .numberOfCallbacks  = sizeof(gpioCallbackFunctions)/sizeof(GPIO_CallbackFxn),
    .intPriority        = (~0)
};

/*
 *  =============================== GPTimer ===============================
 *  Remove unused entries to reduce flash usage both in Board.c and Board.h
 */
#include <ti/drivers/timer/GPTimerCC26XX.h>

GPTimerCC26XX_Object gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMERCOUNT];

const GPTimerCC26XX_HWAttrs gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMERPARTSCOUNT] = {
    { .baseAddr = GPT0_BASE, .intNum = INT_GPT0A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT0, .pinMux = GPT_PIN_0A, },
    { .baseAddr = GPT0_BASE, .intNum = INT_GPT0B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT0, .pinMux = GPT_PIN_0B, },
    { .baseAddr = GPT1_BASE, .intNum = INT_GPT1A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT1, .pinMux = GPT_PIN_1A, },
    { .baseAddr = GPT1_BASE, .intNum = INT_GPT1B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT1, .pinMux = GPT_PIN_1B, },
    { .baseAddr = GPT2_BASE, .intNum = INT_GPT2A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT2, .pinMux = GPT_PIN_2A, },
    { .baseAddr = GPT2_BASE, .intNum = INT_GPT2B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT2, .pinMux = GPT_PIN_2B, },
    { .baseAddr = GPT3_BASE, .intNum = INT_GPT3A, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT3, .pinMux = GPT_PIN_3A, },
    { .baseAddr = GPT3_BASE, .intNum = INT_GPT3B, .intPriority = (~0), .powerMngrId = PowerCC26XX_PERIPH_GPT3, .pinMux = GPT_PIN_3B, },
};

const GPTimerCC26XX_Config GPTimerCC26XX_config[CC2640R2DK_5XD_GPTIMERPARTSCOUNT] = {
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER0], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER0A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER0], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER0B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER1], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER1A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER1], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER1B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER2], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER2A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER2], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER2B], GPT_B },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER3], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER3A], GPT_A },
    { &gptimerCC26XXObjects[CC2640R2DK_5XD_GPTIMER3], &gptimerCC26xxHWAttrs[CC2640R2DK_5XD_GPTIMER3B], GPT_B },
};

/*
 *  =============================== PIN ===============================
 */
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>

const PIN_Config BoardGpioInitTable[] = {

    CC2640R2DK_5XD_PIN_LED3 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,  /* LED initially off */
    CC2640R2DK_5XD_PIN_LED4 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,  /* LED initially off */

    CC2640R2DK_5XD_3V3_EN | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL,                 /* 3V3 domain off initially */
    CC2640R2DK_5XD_UART_TX | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL,               /* UART TX pin at inactive level */

    PIN_TERMINATE
};

const PINCC26XX_HWAttrs PINCC26XX_hwAttrs = {
    .intPriority = ~0,
    .swiPriority = 0
};

/*
 *  =============================== PWM ===============================
 *  Remove unused entries to reduce flash usage both in Board.c and Board.h
 */
#include <ti/drivers/PWM.h>
#include <ti/drivers/pwm/PWMTimerCC26XX.h>

PWMTimerCC26XX_Object pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWMCOUNT];

const PWMTimerCC26XX_HwAttrs pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWMCOUNT] = {
    { .pwmPin = CC2640R2DK_5XD_PWMPIN0, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER0A },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN1, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER0B },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN2, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER1A },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN3, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER1B },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN4, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER2A },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN5, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER2B },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN6, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER3A },
    { .pwmPin = CC2640R2DK_5XD_PWMPIN7, .gpTimerUnit = CC2640R2DK_5XD_GPTIMER3B },
};

const PWM_Config PWM_config[CC2640R2DK_5XD_PWMCOUNT] = {
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM0], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM0] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM1], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM1] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM2], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM2] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM3], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM3] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM4], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM4] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM5], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM5] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM6], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM6] },
    { &PWMTimerCC26XX_fxnTable, &pwmtimerCC26xxObjects[CC2640R2DK_5XD_PWM7], &pwmtimerCC26xxHWAttrs[CC2640R2DK_5XD_PWM7] },
};

const uint_least8_t PWM_count = CC2640R2DK_5XD_PWMCOUNT;

/*
 *  =============================== RF Driver ===============================
 *  Note: The BLE-Stack requires RF SWI priorities to be set to 5.
 */
#include <ti/drivers/rf/RF.h>

const RFCC26XX_HWAttrs RFCC26XX_hwAttrs = {
    .hwiCpe0Priority = ~0,
    .hwiHwPriority   = ~0,
    .swiCpe0Priority =  5,
    .swiHwPriority   =  5,
};

/*
 *  =============================== SPI DMA ===============================
 */
#include <ti/drivers/SPI.h>
#include <ti/drivers/spi/SPICC26XXDMA.h>

SPICC26XXDMA_Object spiCC26XXDMAObjects[CC2640R2DK_5XD_SPICOUNT];

const SPICC26XXDMA_HWAttrsV1 spiCC26XXDMAHWAttrs[CC2640R2DK_5XD_SPICOUNT] = {
    {
        .baseAddr           = SSI0_BASE,
        .intNum             = INT_SSI0_COMB,
        .intPriority        = ~0,
        .swiPriority        = 0,
        .powerMngrId        = PowerCC26XX_PERIPH_SSI0,
        .defaultTxBufValue  = 0,
        .rxChannelBitMask   = 1<<UDMA_CHAN_SSI0_RX,
        .txChannelBitMask   = 1<<UDMA_CHAN_SSI0_TX,
        .mosiPin            = CC2640R2DK_5XD_SPI0_MOSI,
        .misoPin            = CC2640R2DK_5XD_SPI0_MISO,
        .clkPin             = CC2640R2DK_5XD_SPI0_CLK,
        .csnPin             = CC2640R2DK_5XD_SPI0_CSN
    }
};

const SPI_Config SPI_config[CC2640R2DK_5XD_SPICOUNT] = {
    {
         .fxnTablePtr = &SPICC26XXDMA_fxnTable,
         .object      = &spiCC26XXDMAObjects[CC2640R2DK_5XD_SPI0],
         .hwAttrs     = &spiCC26XXDMAHWAttrs[CC2640R2DK_5XD_SPI0]
    }
};

const uint_least8_t SPI_count = CC2640R2DK_5XD_SPICOUNT;

/*
 *  =============================== I2C ===============================
*/
#include <ti/drivers/I2C.h>
#include <ti/drivers/i2c/I2CCC26XX.h>

I2CCC26XX_Object i2cCC26xxObjects[CC2640R2DK_5XD_I2CCOUNT];

const I2CCC26XX_HWAttrsV1 i2cCC26xxHWAttrs[CC2640R2DK_5XD_I2CCOUNT] = {
    {
        .baseAddr    = I2C0_BASE,
        .powerMngrId = PowerCC26XX_PERIPH_I2C0,
        .intNum      = INT_I2C_IRQ,
        .intPriority = ~0,
        .swiPriority = 0,
        .sdaPin      = CC2640R2_LAUNCHXL_I2C0_SDA0,
        .sclPin      = CC2640R2_LAUNCHXL_I2C0_SCL0,
    }
};

const I2C_Config I2C_config[CC2640R2DK_5XD_I2CCOUNT] = {
    {
        .fxnTablePtr = &I2CCC26XX_fxnTable,
        .object      = &i2cCC26xxObjects[CC2640R2DK_5XD_I2C0],
        .hwAttrs     = &i2cCC26xxHWAttrs[CC2640R2DK_5XD_I2C0]
    },
};

const uint_least8_t I2C_count = CC2640R2DK_5XD_I2CCOUNT;
/*
 *  =============================== UART ===============================
 */
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/UARTCC26XX.h>

UARTCC26XX_Object uartCC26XXObjects[CC2640R2DK_5XD_UARTCOUNT];

const UARTCC26XX_HWAttrsV2 uartCC26XXHWAttrs[CC2640R2DK_5XD_UARTCOUNT] = {
    {
        .baseAddr       = UART0_BASE,
        .powerMngrId    = PowerCC26XX_PERIPH_UART0,
        .intNum         = INT_UART0_COMB,
        .intPriority    = ~0,
        .swiPriority    = 0,
        .txPin          = CC2640R2DK_5XD_UART_TX,
        .rxPin          = CC2640R2DK_5XD_UART_RX,
        .ctsPin         = PIN_UNASSIGNED,
        .rtsPin         = PIN_UNASSIGNED
    }
};

const UART_Config UART_config[CC2640R2DK_5XD_UARTCOUNT] = {
    {
        .fxnTablePtr = &UARTCC26XX_fxnTable,
        .object      = &uartCC26XXObjects[CC2640R2DK_5XD_UART0],
        .hwAttrs     = &uartCC26XXHWAttrs[CC2640R2DK_5XD_UART0]
    },
};

const uint_least8_t UART_count = CC2640R2DK_5XD_UARTCOUNT;

/*
 *  =============================== UDMA ===============================
 */
#include <ti/drivers/dma/UDMACC26XX.h>

UDMACC26XX_Object udmaObjects[CC2640R2DK_5XD_UDMACOUNT];

const UDMACC26XX_HWAttrs udmaHWAttrs[CC2640R2DK_5XD_UDMACOUNT] = {
    {
        .baseAddr    = UDMA0_BASE,
        .powerMngrId = PowerCC26XX_PERIPH_UDMA,
        .intNum      = INT_DMA_ERR,
        .intPriority = ~0
    }
};

const UDMACC26XX_Config UDMACC26XX_config[CC2640R2DK_5XD_UDMACOUNT] = {
    {
         .object  = &udmaObjects[CC2640R2DK_5XD_UDMA0],
         .hwAttrs = &udmaHWAttrs[CC2640R2DK_5XD_UDMA0]
    },
};

/*
 *  =============================== Watchdog ===============================
 */
#include <ti/drivers/Watchdog.h>
#include <ti/drivers/watchdog/WatchdogCC26XX.h>

WatchdogCC26XX_Object watchdogCC26XXObjects[CC2640R2DK_5XD_WATCHDOGCOUNT];

const WatchdogCC26XX_HWAttrs watchdogCC26XXHWAttrs[CC2640R2DK_5XD_WATCHDOGCOUNT] = {
    {
        .baseAddr    = WDT_BASE,
        .reloadValue = 1000 /* Reload value in milliseconds */
    },
};

const Watchdog_Config Watchdog_config[CC2640R2DK_5XD_WATCHDOGCOUNT] = {
    {
        .fxnTablePtr = &WatchdogCC26XX_fxnTable,
        .object      = &watchdogCC26XXObjects[CC2640R2DK_5XD_WATCHDOG0],
        .hwAttrs     = &watchdogCC26XXHWAttrs[CC2640R2DK_5XD_WATCHDOG0]
    },
};

const uint_least8_t Watchdog_count = CC2640R2DK_5XD_WATCHDOGCOUNT;



/*
 *  ========================= TRNG begin ====================================
 */
#include <TRNGCC26XX.h>

/* TRNG objects */
TRNGCC26XX_Object trngCC26XXObjects[CC2640R2DK_5XD_TRNGCOUNT];

/* TRNG configuration structure, describing which pins are to be used */
const TRNGCC26XX_HWAttrs TRNGCC26XXHWAttrs[CC2640R2DK_5XD_TRNGCOUNT] = {
    {
        .powerMngrId    = PowerCC26XX_PERIPH_TRNG,
    }
};

/* TRNG configuration structure */
const TRNGCC26XX_Config TRNGCC26XX_config[] = {
    {
         .object  = &trngCC26XXObjects[0],
         .hwAttrs = &TRNGCC26XXHWAttrs[0]
    },
    {NULL, NULL}
};

/*
 *  ========================= TRNG end ====================================
 */


/*
 *  ======== CC2640R2DK_5XD_initGeneral ========
 */
void CC2640R2DK_5XD_initGeneral(void)
{
    Power_init();

    if ( PIN_init(BoardGpioInitTable) != PIN_SUCCESS) {
        System_abort("Error with PIN_init\n");
    }
}

CC2640R2DK_5XD.h

Thanks and Regard

Rohit