This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2650: Sensor Controller : How to change the inputs to the sensor controller Dynamically?

Part Number: CC2650

Tool/software: TI-RTOS

Hello Sir,

I have a task named FADER and I use this code

 scifOsalInit();
 scifInit(&scifDriverSetup);


    // Main loop
    while (1) {
        // Configure the LED Fader task
        Semaphore_pend(Semaphore_handle(&ledActivated), BIOS_WAIT_FOREVER);
        while (scifWaitOnNbl(0) != SCIF_SUCCESS);
            scifExecuteTasksOnceNbl(BV(SCIF_LED_FADER_TASK_ID));
    }

and if use some values like below  before making the semaphore post

  scifTaskData.ledFader.input.moisture     = 1;
  scifTaskData.ledFader.input.eventType[1] = 1;

the corresponding action is not taking place. I tried the same with cfg and output structure too. Could you please tell me when to use these structure and how to change its input from the main application so that the particular action defined can take place in the senor controller.