This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2560: Acceptable Clock SBC Encoder/Decoder

Part Number: CC2560

I am using the CC2560 assisted Mode.

I would know about the technical parameter for the SBC encoder/decoder firmware in the TI Chps.

My FSync is data expected to run at the 48kHz, but my hardware may be some tolerance in the crystal.

I would like to check, what is the acceptable range for the tolerance, such that the SBC encoder/decoder can accept?

Say, if my clock as at 47.9kHz, or 48.1kHz. I want to know if there is such acceptable range for the clock defined?

If, the clock in some case, the clock is out of the scope, what will the encoder/decoder firmware handle? Will it still work with some jitter, or it will do some adaption, or just discard all the input data?