Tool/software: Code Composer Studio
The bootloader tool "sblAppEx" which offered by TI can run on PC , and realize CC2640 bootloader through UART . However , the CC2640 bootloader must be realized through SPI according to the requirement of my project . How to realize CC2640 bootloader through "sblAppEx" and PC ?
1. "sblAppEx" can run on PC with VC++2010. However, after running "sblAppEx" on PC , only UART COM port can be captured , instead of SPI port . Picture 1 shows the result of "sblAppEx" running on PC .
picture 1
2. Is “bootloader backdoor enable” essential for conducting CC2640 bootloader through SPI?
3. The reference of CC2640 bootloader is shown in picture 2 .
picture 2
4.attachments:
(1)simplelink_cc2640r2_sdk_1_40_00_45 can be downloaded here :
(2)CC2640R2 launchpad can be bought here:
(3)“sblAppEx” can be downloaded here:
5.my developing environment
CCS:Code Composer Studio 7.2.0
SDK:simplelink_cc2640r2_sdk_1_40_00_45
hardware:CC26640R2 launchpad develop kit
VS: Microsoft Visual C++ 2010 Express
OS:win7 64 bit