Part Number: CC2650
Tool/software: TI-RTOS
found a bug in sbl.c which is used to flash the CC2650. I had problems getting msp432P401R + CC2650 + sensorpack example to run and so I reflashed the CC2650 with "simple_np_cc2650bp_uart_pm_sbl_2_02_01_18a_merge.c" and this created new problems in that the power up indication no longer occurred.
So the problem is that the code in sbl.c ... uint8_t SBL_writeImage(SBL_Image *image) has in it the following code that is incorrect (it reduces the imgSize if the last sector IS NOT protected ... is should reduce imgSize if the last sector IS protected.
if (!SBL_isLastSectorProtected())
{
// if the last sector is not protected, do not touch the last sector
imgSize -= SBL_PAGE_SIZE;
}
it should be
if (SBL_isLastSectorProtected())
{
// if the last sector is protected, do not touch the last sector
imgSize -= SBL_PAGE_SIZE;
}