Part Number: LAUNCHXL-CC26X2R1
Tool/software: Code Composer Studio
Hello,
I just got my new CC26X2R1LP. I plugged it into my computer and using the TI cloud IDE I tried to download the BLESimplePeripheral stack, as I have done with other LPs. During the compile process, the IDE paused suggesting that the debugger needs a firmware update. The only option was OK, which I clicked. It warned me to not unplug the device while updating the firmware. After 3 hours, I was convinced that the process had failed. I had no choice but to restart the IDE. I then tried again to download and debug the stack. Compilation completed, but then exited with the "Socket error". No doubt the failed firmware update is the problem. Is there some way to recover? Typically an image of the firmware is saved that can be restored via a combination of button pushes, etc. Is there something like this for this launchpad.
help is appreciated,
Patrick