This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: BUG in Stack: System (M3) hangs up if no new handle available for registering service

Part Number: CC2640R2F


Hello,

we have got a use case where we are deregister and register a service from time to time. If the system runs over years the following case could happen in reality when the system is in customer hands:

After my last question relating to register and deregister a service, my additional question relating to the stack: "what whill happen if the handle id reaches the uint16_t 0xFFFF" was not answered. Thus I tried it by myself. I continuously register and deregister the same service and output the handle ID of the service to the UART. My service has got 6 items so the stack increments the handle ID by 6 after registering my service.

After deregistering the service handle ID 3358, no new service can be registered. Furthermore the M3 CPU hangs up after initiating the registering process. The M0 CPU is still running until a new BLE event happens. Then the complete system is dead. The only solution is to reset the whole device. I read about it in an older forum post from 2014. So I assume, Ti did not fix that BLE stack bug in the meantime of 4 years?

Do you have a smoother solution except resetting the whole device?

Thanks you.
Regards
Andre

  • Hi Andre,

    I did not see any inquries related to: "what whill happen if the handle id reaches the uint16_t 0xFFFF"
    but I can answer that question for you now. If the number of attributes in your service is greater than ( GATT_MAX_HANDLE - currentMaxHdl) + 1 ) then GATTServApp_RegisterService() will return failure.

    Regarding the failure, do you have a set of code that reproduces the issue, perhaps on the simple_peripheral project?
    Please show us where to place the code and what to change and we can investigate further for you.
  • Hi Sean,

    here is the post I am refering to: e2e.ti.com/.../272241

    -> While continuously registering and deregistering the same service, the handle will increase each cycle. So my question is: Do you have a solution to decrease the handle after deregistering a service? Because if it is not possible to decrease the handle, the only way to get it down is a full device reset. But this would be a very messy solution...

    -> I have a set of code. It uses simple_peripheral project. In more detail its a modified project_zero project. In ProjectZero_taskFxn() I call periodically (every 200 ms):
    if (events & SC_PERIODIC_EVT)
    {
    // Perform periodic application task
    static uint8_t status = 1;
    if (status == 1)
    {
    PIN_setOutputValue(ledPinHandle, Board_RLED, 1);
    status = 0;
    DebugService_RemoveService();

    }
    else
    {
    PIN_setOutputValue(ledPinHandle, Board_RLED, 0);
    status = 1;
    DebugService_AddService(selfEntity); // This service I created with Bluetooth Developer Studio and Ti Plugin
    }
    }

    In an extern file i defined the RemoveService:
    extern void DebugService_RemoveService(void)
    {
    uint16_t DebugService_handle = GATT_SERVICE_HANDLE(DEBUG_SERVICEAttrTbl);
    Log_info1("Remove Service with handle: %d", (IArg)DebugService_handle);
    GATTServApp_DeregisterService(DebugService_handle, NULL);
    }
  • Are you working on a solution? Please keep me up to date.

    Regards
    Andre
  • Hi Andre,

    My apologies for not responding. I have been looking into this issue and have the following update for you.

    1. Regarding decreasing the handle. It does unfortunately appear that it is still not possible to reset the currently handle that is being used by the GATT Server. This number is set to 0 by the BSS initialization when the device boots and only increases as services are added. When services are removed, the active handle does not decrease. I have filed a ticket with our R&D team to request that feature as I understand it is critical for adding and removing services dynamically

    2.  I am not able to reproduce the system hang that you describe. I have used the CC2640R2 SDK 1.50.00.58 with sample app simple_peripheral and simple_gatt_profile. I modified the simple gatt profile to add a function to deregister the service as we have discussed in another thread.

    In the periodic task function handler I add and remove the service just as you do in your comment above. However, the system does not hang. I have let the demo run and eventually the handle reaches the max handle and the service cannot be re added. For me, using the attached sample code, it stopped at 65512 with error status of 1 returned from the GATT server. This error code is consistent with the server not having enough available handles to assign to your new service.

    I have attached the sample code that I used (simple_peripheral.c, simple_gatt_profile.c,h) to this thread that I used.

    I do not have the code for your DebugService_AddService function, but if I am suspicious of a memory leak if you have any notifiable or indictable characteristics.  For example I used the Bluetooth Developer Studio plugin to generate a sample service. It contained the following code in the _addService function:

      // Allocate Client Characteristic Configuration table
      dns_MyChar1Config = (gattCharCfg_t *)ICall_malloc( sizeof(gattCharCfg_t) * linkDBNumConns );
      if ( dns_MyChar1Config == NULL )
      {
        return ( bleMemAllocError );
      }

    From the snippet above, the services generated by BDS will call malloc for each CCCD, If you have CCCDs in your generated service, you will need to free them as I am doing in the attached SimpleProfile_RemoveService().

    /******************************************************************************
    
     @file       simple_gatt_profile.c
    
     @brief This file contains the Simple GATT profile sample GATT service profile
            for use with the BLE sample application.
    
     Group: CMCU, SCS
     Target Device: CC2640R2
    
     ******************************************************************************
    
     Copyright (c) 2010-2017, Texas Instruments Incorporated
     All rights reserved.
    
     Redistribution and use in source and binary forms, with or without
     modification, are permitted provided that the following conditions
     are met:
    
     *  Redistributions of source code must retain the above copyright
        notice, this list of conditions and the following disclaimer.
    
     *  Redistributions in binary form must reproduce the above copyright
        notice, this list of conditions and the following disclaimer in the
        documentation and/or other materials provided with the distribution.
    
     *  Neither the name of Texas Instruments Incorporated nor the names of
        its contributors may be used to endorse or promote products derived
        from this software without specific prior written permission.
    
     THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    
     ******************************************************************************
     Release Name: simplelink_cc2640r2_sdk_01_50_00_58_s
     Release Date: 2017-10-17 18:50:56
     *****************************************************************************/
    
    /*********************************************************************
     * INCLUDES
     */
    #include <string.h>
    #include <icall.h>
    #include "util.h"
    /* This Header file contains all BLE API and icall structure definition */
    #include "icall_ble_api.h"
    
    #include "simple_gatt_profile.h"
    
    /*********************************************************************
     * MACROS
     */
    
    /*********************************************************************
     * CONSTANTS
     */
    
    #define SERVAPP_NUM_ATTR_SUPPORTED        17
    
    /*********************************************************************
     * TYPEDEFS
     */
    
    /*********************************************************************
     * GLOBAL VARIABLES
     */
    // Simple GATT Profile Service UUID: 0xFFF0
    CONST uint8 simpleProfileServUUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_SERV_UUID), HI_UINT16(SIMPLEPROFILE_SERV_UUID)
    };
    
    // Characteristic 1 UUID: 0xFFF1
    CONST uint8 simpleProfilechar1UUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_CHAR1_UUID), HI_UINT16(SIMPLEPROFILE_CHAR1_UUID)
    };
    
    // Characteristic 2 UUID: 0xFFF2
    CONST uint8 simpleProfilechar2UUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_CHAR2_UUID), HI_UINT16(SIMPLEPROFILE_CHAR2_UUID)
    };
    
    // Characteristic 3 UUID: 0xFFF3
    CONST uint8 simpleProfilechar3UUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_CHAR3_UUID), HI_UINT16(SIMPLEPROFILE_CHAR3_UUID)
    };
    
    // Characteristic 4 UUID: 0xFFF4
    CONST uint8 simpleProfilechar4UUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_CHAR4_UUID), HI_UINT16(SIMPLEPROFILE_CHAR4_UUID)
    };
    
    // Characteristic 5 UUID: 0xFFF5
    CONST uint8 simpleProfilechar5UUID[ATT_BT_UUID_SIZE] =
    {
      LO_UINT16(SIMPLEPROFILE_CHAR5_UUID), HI_UINT16(SIMPLEPROFILE_CHAR5_UUID)
    };
    
    /*********************************************************************
     * EXTERNAL VARIABLES
     */
    
    /*********************************************************************
     * EXTERNAL FUNCTIONS
     */
    
    /*********************************************************************
     * LOCAL VARIABLES
     */
    
    static simpleProfileCBs_t *simpleProfile_AppCBs = NULL;
    
    /*********************************************************************
     * Profile Attributes - variables
     */
    
    // Simple Profile Service attribute
    static CONST gattAttrType_t simpleProfileService = { ATT_BT_UUID_SIZE, simpleProfileServUUID };
    
    
    // Simple Profile Characteristic 1 Properties
    static uint8 simpleProfileChar1Props = GATT_PROP_READ | GATT_PROP_WRITE;
    
    // Characteristic 1 Value
    static uint8 simpleProfileChar1 = 0;
    
    // Simple Profile Characteristic 1 User Description
    static uint8 simpleProfileChar1UserDesp[17] = "Characteristic 1";
    
    
    // Simple Profile Characteristic 2 Properties
    static uint8 simpleProfileChar2Props = GATT_PROP_READ;
    
    // Characteristic 2 Value
    static uint8 simpleProfileChar2 = 0;
    
    // Simple Profile Characteristic 2 User Description
    static uint8 simpleProfileChar2UserDesp[17] = "Characteristic 2";
    
    
    // Simple Profile Characteristic 3 Properties
    static uint8 simpleProfileChar3Props = GATT_PROP_WRITE;
    
    // Characteristic 3 Value
    static uint8 simpleProfileChar3 = 0;
    
    // Simple Profile Characteristic 3 User Description
    static uint8 simpleProfileChar3UserDesp[17] = "Characteristic 3";
    
    
    // Simple Profile Characteristic 4 Properties
    static uint8 simpleProfileChar4Props = GATT_PROP_NOTIFY;
    
    // Characteristic 4 Value
    static uint8 simpleProfileChar4 = 0;
    
    // Simple Profile Characteristic 4 Configuration Each client has its own
    // instantiation of the Client Characteristic Configuration. Reads of the
    // Client Characteristic Configuration only shows the configuration for
    // that client and writes only affect the configuration of that client.
    static gattCharCfg_t *simpleProfileChar4Config;
    
    // Simple Profile Characteristic 4 User Description
    static uint8 simpleProfileChar4UserDesp[17] = "Characteristic 4";
    
    
    // Simple Profile Characteristic 5 Properties
    static uint8 simpleProfileChar5Props = GATT_PROP_READ;
    
    // Characteristic 5 Value
    static uint8 simpleProfileChar5[SIMPLEPROFILE_CHAR5_LEN] = { 0, 0, 0, 0, 0 };
    
    // Simple Profile Characteristic 5 User Description
    static uint8 simpleProfileChar5UserDesp[17] = "Characteristic 5";
    
    /*********************************************************************
     * Profile Attributes - Table
     */
    
    static gattAttribute_t simpleProfileAttrTbl[SERVAPP_NUM_ATTR_SUPPORTED] =
    {
      // Simple Profile Service
      {
        { ATT_BT_UUID_SIZE, primaryServiceUUID }, /* type */
        GATT_PERMIT_READ,                         /* permissions */
        0,                                        /* handle */
        (uint8 *)&simpleProfileService            /* pValue */
      },
    
        // Characteristic 1 Declaration
        {
          { ATT_BT_UUID_SIZE, characterUUID },
          GATT_PERMIT_READ,
          0,
          &simpleProfileChar1Props
        },
    
          // Characteristic Value 1
          {
            { ATT_BT_UUID_SIZE, simpleProfilechar1UUID },
            GATT_PERMIT_READ | GATT_PERMIT_WRITE,
            0,
            &simpleProfileChar1
          },
    
          // Characteristic 1 User Description
          {
            { ATT_BT_UUID_SIZE, charUserDescUUID },
            GATT_PERMIT_READ,
            0,
            simpleProfileChar1UserDesp
          },
    
        // Characteristic 2 Declaration
        {
          { ATT_BT_UUID_SIZE, characterUUID },
          GATT_PERMIT_READ,
          0,
          &simpleProfileChar2Props
        },
    
          // Characteristic Value 2
          {
            { ATT_BT_UUID_SIZE, simpleProfilechar2UUID },
            GATT_PERMIT_READ,
            0,
            &simpleProfileChar2
          },
    
          // Characteristic 2 User Description
          {
            { ATT_BT_UUID_SIZE, charUserDescUUID },
            GATT_PERMIT_READ,
            0,
            simpleProfileChar2UserDesp
          },
    
        // Characteristic 3 Declaration
        {
          { ATT_BT_UUID_SIZE, characterUUID },
          GATT_PERMIT_READ,
          0,
          &simpleProfileChar3Props
        },
    
          // Characteristic Value 3
          {
            { ATT_BT_UUID_SIZE, simpleProfilechar3UUID },
            GATT_PERMIT_WRITE,
            0,
            &simpleProfileChar3
          },
    
          // Characteristic 3 User Description
          {
            { ATT_BT_UUID_SIZE, charUserDescUUID },
            GATT_PERMIT_READ,
            0,
            simpleProfileChar3UserDesp
          },
    
        // Characteristic 4 Declaration
        {
          { ATT_BT_UUID_SIZE, characterUUID },
          GATT_PERMIT_READ,
          0,
          &simpleProfileChar4Props
        },
    
          // Characteristic Value 4
          {
            { ATT_BT_UUID_SIZE, simpleProfilechar4UUID },
            0,
            0,
            &simpleProfileChar4
          },
    
          // Characteristic 4 configuration
          {
            { ATT_BT_UUID_SIZE, clientCharCfgUUID },
            GATT_PERMIT_READ | GATT_PERMIT_WRITE,
            0,
            (uint8 *)&simpleProfileChar4Config
          },
    
          // Characteristic 4 User Description
          {
            { ATT_BT_UUID_SIZE, charUserDescUUID },
            GATT_PERMIT_READ,
            0,
            simpleProfileChar4UserDesp
          },
    
        // Characteristic 5 Declaration
        {
          { ATT_BT_UUID_SIZE, characterUUID },
          GATT_PERMIT_READ,
          0,
          &simpleProfileChar5Props
        },
    
          // Characteristic Value 5
          {
            { ATT_BT_UUID_SIZE, simpleProfilechar5UUID },
            GATT_PERMIT_AUTHEN_READ,
            0,
            simpleProfileChar5
          },
    
          // Characteristic 5 User Description
          {
            { ATT_BT_UUID_SIZE, charUserDescUUID },
            GATT_PERMIT_READ,
            0,
            simpleProfileChar5UserDesp
          },
    };
    
    /*********************************************************************
     * LOCAL FUNCTIONS
     */
    static bStatus_t simpleProfile_ReadAttrCB(uint16_t connHandle,
                                              gattAttribute_t *pAttr,
                                              uint8_t *pValue, uint16_t *pLen,
                                              uint16_t offset, uint16_t maxLen,
                                              uint8_t method);
    static bStatus_t simpleProfile_WriteAttrCB(uint16_t connHandle,
                                               gattAttribute_t *pAttr,
                                               uint8_t *pValue, uint16_t len,
                                               uint16_t offset, uint8_t method);
    
    /*********************************************************************
     * PROFILE CALLBACKS
     */
    
    // Simple Profile Service Callbacks
    // Note: When an operation on a characteristic requires authorization and
    // pfnAuthorizeAttrCB is not defined for that characteristic's service, the
    // Stack will report a status of ATT_ERR_UNLIKELY to the client.  When an
    // operation on a characteristic requires authorization the Stack will call
    // pfnAuthorizeAttrCB to check a client's authorization prior to calling
    // pfnReadAttrCB or pfnWriteAttrCB, so no checks for authorization need to be
    // made within these functions.
    CONST gattServiceCBs_t simpleProfileCBs =
    {
      simpleProfile_ReadAttrCB,  // Read callback function pointer
      simpleProfile_WriteAttrCB, // Write callback function pointer
      NULL                       // Authorization callback function pointer
    };
    
    /*********************************************************************
     * PUBLIC FUNCTIONS
     */
    
    /*********************************************************************
     * @fn      SimpleProfile_AddService
     *
     * @brief   Initializes the Simple Profile service by registering
     *          GATT attributes with the GATT server.
     *
     * @param   services - services to add. This is a bit map and can
     *                     contain more than one service.
     *
     * @return  Success or Failure
     */
    bStatus_t SimpleProfile_AddService( uint32 services )
    {
      uint8 status;
    
      // Allocate Client Characteristic Configuration table
      simpleProfileChar4Config = (gattCharCfg_t *)ICall_malloc( sizeof(gattCharCfg_t) *
                                                                linkDBNumConns );
      if ( simpleProfileChar4Config == NULL )
      {
        return ( bleMemAllocError );
      }
    
      // Initialize Client Characteristic Configuration attributes
      GATTServApp_InitCharCfg( INVALID_CONNHANDLE, simpleProfileChar4Config );
    
      if ( services & SIMPLEPROFILE_SERVICE )
      {
        // Register GATT attribute list and CBs with GATT Server App
        status = GATTServApp_RegisterService( simpleProfileAttrTbl,
                                              GATT_NUM_ATTRS( simpleProfileAttrTbl ),
                                              GATT_MAX_ENCRYPT_KEY_SIZE,
                                              &simpleProfileCBs );
      }
      else
      {
        status = SUCCESS;
      }
    
      return ( status );
    }
    
    
    /*********************************************************************
     * @fn      SimpleProfile_RemoveService
     *
     * @brief   Deregisters the service with the GATT server.
     *
     * @param   services - services to add. This is a bit map and can
     *                     contain more than one service.
     *
     * @return  Success or Failure
     */
    uint16_t SimpleProfile_RemoveService(void)
    {
      uint16_t handle = GATT_SERVICE_HANDLE(simpleProfileAttrTbl);
      GATTServApp_DeregisterService(handle, NULL);
    
      if(simpleProfileChar4Config != NULL)
      {
        ICall_free(simpleProfileChar4Config);
      }
      return handle;
    
    }
    
    /*********************************************************************
     * @fn      SimpleProfile_RegisterAppCBs
     *
     * @brief   Registers the application callback function. Only call
     *          this function once.
     *
     * @param   callbacks - pointer to application callbacks.
     *
     * @return  SUCCESS or bleAlreadyInRequestedMode
     */
    bStatus_t SimpleProfile_RegisterAppCBs( simpleProfileCBs_t *appCallbacks )
    {
      if ( appCallbacks )
      {
        simpleProfile_AppCBs = appCallbacks;
    
        return ( SUCCESS );
      }
      else
      {
        return ( bleAlreadyInRequestedMode );
      }
    }
    
    /*********************************************************************
     * @fn      SimpleProfile_SetParameter
     *
     * @brief   Set a Simple Profile parameter.
     *
     * @param   param - Profile parameter ID
     * @param   len - length of data to write
     * @param   value - pointer to data to write.  This is dependent on
     *          the parameter ID and WILL be cast to the appropriate
     *          data type (example: data type of uint16 will be cast to
     *          uint16 pointer).
     *
     * @return  bStatus_t
     */
    bStatus_t SimpleProfile_SetParameter( uint8 param, uint8 len, void *value )
    {
      bStatus_t ret = SUCCESS;
      switch ( param )
      {
        case SIMPLEPROFILE_CHAR1:
          if ( len == sizeof ( uint8 ) )
          {
            simpleProfileChar1 = *((uint8*)value);
          }
          else
          {
            ret = bleInvalidRange;
          }
          break;
    
        case SIMPLEPROFILE_CHAR2:
          if ( len == sizeof ( uint8 ) )
          {
            simpleProfileChar2 = *((uint8*)value);
          }
          else
          {
            ret = bleInvalidRange;
          }
          break;
    
        case SIMPLEPROFILE_CHAR3:
          if ( len == sizeof ( uint8 ) )
          {
            simpleProfileChar3 = *((uint8*)value);
          }
          else
          {
            ret = bleInvalidRange;
          }
          break;
    
        case SIMPLEPROFILE_CHAR4:
          if ( len == sizeof ( uint8 ) )
          {
            simpleProfileChar4 = *((uint8*)value);
    
            // See if Notification has been enabled
            GATTServApp_ProcessCharCfg( simpleProfileChar4Config, &simpleProfileChar4, FALSE,
                                        simpleProfileAttrTbl, GATT_NUM_ATTRS( simpleProfileAttrTbl ),
                                        INVALID_TASK_ID, simpleProfile_ReadAttrCB );
          }
          else
          {
            ret = bleInvalidRange;
          }
          break;
    
        case SIMPLEPROFILE_CHAR5:
          if ( len == SIMPLEPROFILE_CHAR5_LEN )
          {
            VOID memcpy( simpleProfileChar5, value, SIMPLEPROFILE_CHAR5_LEN );
          }
          else
          {
            ret = bleInvalidRange;
          }
          break;
    
        default:
          ret = INVALIDPARAMETER;
          break;
      }
    
      return ( ret );
    }
    
    /*********************************************************************
     * @fn      SimpleProfile_GetParameter
     *
     * @brief   Get a Simple Profile parameter.
     *
     * @param   param - Profile parameter ID
     * @param   value - pointer to data to put.  This is dependent on
     *          the parameter ID and WILL be cast to the appropriate
     *          data type (example: data type of uint16 will be cast to
     *          uint16 pointer).
     *
     * @return  bStatus_t
     */
    bStatus_t SimpleProfile_GetParameter( uint8 param, void *value )
    {
      bStatus_t ret = SUCCESS;
      switch ( param )
      {
        case SIMPLEPROFILE_CHAR1:
          *((uint8*)value) = simpleProfileChar1;
          break;
    
        case SIMPLEPROFILE_CHAR2:
          *((uint8*)value) = simpleProfileChar2;
          break;
    
        case SIMPLEPROFILE_CHAR3:
          *((uint8*)value) = simpleProfileChar3;
          break;
    
        case SIMPLEPROFILE_CHAR4:
          *((uint8*)value) = simpleProfileChar4;
          break;
    
        case SIMPLEPROFILE_CHAR5:
          VOID memcpy( value, simpleProfileChar5, SIMPLEPROFILE_CHAR5_LEN );
          break;
    
        default:
          ret = INVALIDPARAMETER;
          break;
      }
    
      return ( ret );
    }
    
    /*********************************************************************
     * @fn          simpleProfile_ReadAttrCB
     *
     * @brief       Read an attribute.
     *
     * @param       connHandle - connection message was received on
     * @param       pAttr - pointer to attribute
     * @param       pValue - pointer to data to be read
     * @param       pLen - length of data to be read
     * @param       offset - offset of the first octet to be read
     * @param       maxLen - maximum length of data to be read
     * @param       method - type of read message
     *
     * @return      SUCCESS, blePending or Failure
     */
    static bStatus_t simpleProfile_ReadAttrCB(uint16_t connHandle,
                                              gattAttribute_t *pAttr,
                                              uint8_t *pValue, uint16_t *pLen,
                                              uint16_t offset, uint16_t maxLen,
                                              uint8_t method)
    {
      bStatus_t status = SUCCESS;
    
      // Make sure it's not a blob operation (no attributes in the profile are long)
      if ( offset > 0 )
      {
        return ( ATT_ERR_ATTR_NOT_LONG );
      }
    
      if ( pAttr->type.len == ATT_BT_UUID_SIZE )
      {
        // 16-bit UUID
        uint16 uuid = BUILD_UINT16( pAttr->type.uuid[0], pAttr->type.uuid[1]);
        switch ( uuid )
        {
          // No need for "GATT_SERVICE_UUID" or "GATT_CLIENT_CHAR_CFG_UUID" cases;
          // gattserverapp handles those reads
    
          // characteristics 1 and 2 have read permissions
          // characteritisc 3 does not have read permissions; therefore it is not
          //   included here
          // characteristic 4 does not have read permissions, but because it
          //   can be sent as a notification, it is included here
          case SIMPLEPROFILE_CHAR1_UUID:
          case SIMPLEPROFILE_CHAR2_UUID:
          case SIMPLEPROFILE_CHAR4_UUID:
            *pLen = 1;
            pValue[0] = *pAttr->pValue;
            break;
    
          case SIMPLEPROFILE_CHAR5_UUID:
            *pLen = SIMPLEPROFILE_CHAR5_LEN;
            VOID memcpy( pValue, pAttr->pValue, SIMPLEPROFILE_CHAR5_LEN );
            break;
    
          default:
            // Should never get here! (characteristics 3 and 4 do not have read permissions)
            *pLen = 0;
            status = ATT_ERR_ATTR_NOT_FOUND;
            break;
        }
      }
      else
      {
        // 128-bit UUID
        *pLen = 0;
        status = ATT_ERR_INVALID_HANDLE;
      }
    
      return ( status );
    }
    
    /*********************************************************************
     * @fn      simpleProfile_WriteAttrCB
     *
     * @brief   Validate attribute data prior to a write operation
     *
     * @param   connHandle - connection message was received on
     * @param   pAttr - pointer to attribute
     * @param   pValue - pointer to data to be written
     * @param   len - length of data
     * @param   offset - offset of the first octet to be written
     * @param   method - type of write message
     *
     * @return  SUCCESS, blePending or Failure
     */
    static bStatus_t simpleProfile_WriteAttrCB(uint16_t connHandle,
                                               gattAttribute_t *pAttr,
                                               uint8_t *pValue, uint16_t len,
                                               uint16_t offset, uint8_t method)
    {
      bStatus_t status = SUCCESS;
      uint8 notifyApp = 0xFF;
    
      if ( pAttr->type.len == ATT_BT_UUID_SIZE )
      {
        // 16-bit UUID
        uint16 uuid = BUILD_UINT16( pAttr->type.uuid[0], pAttr->type.uuid[1]);
        switch ( uuid )
        {
          case SIMPLEPROFILE_CHAR1_UUID:
          case SIMPLEPROFILE_CHAR3_UUID:
    
            //Validate the value
            // Make sure it's not a blob oper
            if ( offset == 0 )
            {
              if ( len != 1 )
              {
                status = ATT_ERR_INVALID_VALUE_SIZE;
              }
            }
            else
            {
              status = ATT_ERR_ATTR_NOT_LONG;
            }
    
            //Write the value
            if ( status == SUCCESS )
            {
              uint8 *pCurValue = (uint8 *)pAttr->pValue;
              *pCurValue = pValue[0];
    
              if( pAttr->pValue == &simpleProfileChar1 )
              {
                notifyApp = SIMPLEPROFILE_CHAR1;
              }
              else
              {
                notifyApp = SIMPLEPROFILE_CHAR3;
              }
            }
    
            break;
    
          case GATT_CLIENT_CHAR_CFG_UUID:
            status = GATTServApp_ProcessCCCWriteReq( connHandle, pAttr, pValue, len,
                                                     offset, GATT_CLIENT_CFG_NOTIFY );
            break;
    
          default:
            // Should never get here! (characteristics 2 and 4 do not have write permissions)
            status = ATT_ERR_ATTR_NOT_FOUND;
            break;
        }
      }
      else
      {
        // 128-bit UUID
        status = ATT_ERR_INVALID_HANDLE;
      }
    
      // If a characteristic value changed then callback function to notify application of change
      if ( (notifyApp != 0xFF ) && simpleProfile_AppCBs && simpleProfile_AppCBs->pfnSimpleProfileChange )
      {
        simpleProfile_AppCBs->pfnSimpleProfileChange( notifyApp );
      }
    
      return ( status );
    }
    
    /*********************************************************************
    *********************************************************************/
    
    0447.simple_gatt_profile.h
    /******************************************************************************
    
     @file       simple_peripheral.c
    
     @brief This file contains the Simple Peripheral sample application for use
            with the CC2650 Bluetooth Low Energy Protocol Stack.
    
     Group: CMCU, SCS
     Target Device: CC2640R2
    
     ******************************************************************************
    
     Copyright (c) 2013-2017, Texas Instruments Incorporated
     All rights reserved.
    
     Redistribution and use in source and binary forms, with or without
     modification, are permitted provided that the following conditions
     are met:
    
     *  Redistributions of source code must retain the above copyright
        notice, this list of conditions and the following disclaimer.
    
     *  Redistributions in binary form must reproduce the above copyright
        notice, this list of conditions and the following disclaimer in the
        documentation and/or other materials provided with the distribution.
    
     *  Neither the name of Texas Instruments Incorporated nor the names of
        its contributors may be used to endorse or promote products derived
        from this software without specific prior written permission.
    
     THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    
     ******************************************************************************
     Release Name: simplelink_cc2640r2_sdk_01_50_00_58_s
     Release Date: 2017-10-17 18:50:56
     *****************************************************************************/
    
    /*********************************************************************
     * INCLUDES
     */
    #include <string.h>
    
    #include <ti/sysbios/knl/Task.h>
    #include <ti/sysbios/knl/Clock.h>
    #include <ti/sysbios/knl/Event.h>
    #include <ti/sysbios/knl/Queue.h>
    #include <ti/display/Display.h>
    
    #if defined( USE_FPGA ) || defined( DEBUG_SW_TRACE )
    #include <driverlib/ioc.h>
    #endif // USE_FPGA | DEBUG_SW_TRACE
    
    #include <icall.h>
    #include "util.h"
    /* This Header file contains all BLE API and icall structure definition */
    #include "icall_ble_api.h"
    
    #include "devinfoservice.h"
    #include "simple_gatt_profile.h"
    #include "ll_common.h"
    
    #include "peripheral.h"
    
    #ifdef USE_RCOSC
    #include "rcosc_calibration.h"
    #endif //USE_RCOSC
    
    #include "board_key.h"
    
    #include "board.h"
    
    #include "simple_peripheral.h"
    
    /*********************************************************************
     * CONSTANTS
     */
    
    // Advertising interval when device is discoverable (units of 625us, 160=100ms)
    #define DEFAULT_ADVERTISING_INTERVAL          160
    
    // General discoverable mode: advertise indefinitely
    #define DEFAULT_DISCOVERABLE_MODE             GAP_ADTYPE_FLAGS_GENERAL
    
    // Minimum connection interval (units of 1.25ms, 80=100ms) for automatic
    // parameter update request
    #define DEFAULT_DESIRED_MIN_CONN_INTERVAL     80
    
    // Maximum connection interval (units of 1.25ms, 800=1000ms) for automatic
    // parameter update request
    #define DEFAULT_DESIRED_MAX_CONN_INTERVAL     800
    
    // Slave latency to use for automatic parameter update request
    #define DEFAULT_DESIRED_SLAVE_LATENCY         0
    
    // Supervision timeout value (units of 10ms, 1000=10s) for automatic parameter
    // update request
    #define DEFAULT_DESIRED_CONN_TIMEOUT          1000
    
    // After the connection is formed, the peripheral waits until the central
    // device asks for its preferred connection parameters
    #define DEFAULT_ENABLE_UPDATE_REQUEST         GAPROLE_LINK_PARAM_UPDATE_WAIT_REMOTE_PARAMS
    
    // Connection Pause Peripheral time value (in seconds)
    #define DEFAULT_CONN_PAUSE_PERIPHERAL         6
    
    // How often to perform periodic event (in msec)
    #define SBP_PERIODIC_EVT_PERIOD               200
    
    // Application specific event ID for HCI Connection Event End Events
    #define SBP_HCI_CONN_EVT_END_EVT              0x0001
    
    // Type of Display to open
    #if !defined(Display_DISABLE_ALL)
      #if defined(BOARD_DISPLAY_USE_LCD) && (BOARD_DISPLAY_USE_LCD!=0)
        #define SBP_DISPLAY_TYPE Display_Type_LCD
      #elif defined (BOARD_DISPLAY_USE_UART) && (BOARD_DISPLAY_USE_UART!=0)
        #define SBP_DISPLAY_TYPE Display_Type_UART
      #else // !BOARD_DISPLAY_USE_LCD && !BOARD_DISPLAY_USE_UART
        #define SBP_DISPLAY_TYPE 0 // Option not supported
      #endif // BOARD_DISPLAY_USE_LCD && BOARD_DISPLAY_USE_UART
    #else // BOARD_DISPLAY_USE_LCD && BOARD_DISPLAY_USE_UART
      #define SBP_DISPLAY_TYPE 0 // No Display
    #endif // !Display_DISABLE_ALL
    
    // Task configuration
    #define SBP_TASK_PRIORITY                     1
    
    #ifndef SBP_TASK_STACK_SIZE
    #define SBP_TASK_STACK_SIZE                   644
    #endif
    
    // Application events
    #define SBP_STATE_CHANGE_EVT                  0x0001
    #define SBP_CHAR_CHANGE_EVT                   0x0002
    #define SBP_PAIRING_STATE_EVT                 0x0004
    #define SBP_PASSCODE_NEEDED_EVT               0x0008
    
    // Internal Events for RTOS application
    #define SBP_ICALL_EVT                         ICALL_MSG_EVENT_ID // Event_Id_31
    #define SBP_QUEUE_EVT                         UTIL_QUEUE_EVENT_ID // Event_Id_30
    #define SBP_PERIODIC_EVT                      Event_Id_00
    
    // Bitwise OR of all events to pend on
    #define SBP_ALL_EVENTS                        (SBP_ICALL_EVT        | \
                                                   SBP_QUEUE_EVT        | \
                                                   SBP_PERIODIC_EVT)
    
    /*********************************************************************
     * TYPEDEFS
     */
    
    // App event passed from profiles.
    typedef struct
    {
      appEvtHdr_t hdr;  // event header.
      uint8_t *pData;  // event data
    } sbpEvt_t;
    
    /*********************************************************************
     * GLOBAL VARIABLES
     */
    
    // Display Interface
    Display_Handle dispHandle = NULL;
    
    /*********************************************************************
     * LOCAL VARIABLES
     */
    
    // Entity ID globally used to check for source and/or destination of messages
    static ICall_EntityID selfEntity;
    
    // Event globally used to post local events and pend on system and
    // local events.
    static ICall_SyncHandle syncEvent;
    
    // Clock instances for internal periodic events.
    static Clock_Struct periodicClock;
    
    // Queue object used for app messages
    static Queue_Struct appMsg;
    static Queue_Handle appMsgQueue;
    
    // Task configuration
    Task_Struct sbpTask;
    Char sbpTaskStack[SBP_TASK_STACK_SIZE];
    
    // Scan response data (max size = 31 bytes)
    static uint8_t scanRspData[] =
    {
      // complete name
      0x14,   // length of this data
      GAP_ADTYPE_LOCAL_NAME_COMPLETE,
      'S',
      'i',
      'm',
      'p',
      'l',
      'e',
      'B',
      'L',
      'E',
      'P',
      'e',
      'r',
      'i',
      'p',
      'h',
      'e',
      'r',
      'a',
      'l',
    
      // connection interval range
      0x05,   // length of this data
      GAP_ADTYPE_SLAVE_CONN_INTERVAL_RANGE,
      LO_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL),   // 100ms
      HI_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL),
      LO_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL),   // 1s
      HI_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL),
    
      // Tx power level
      0x02,   // length of this data
      GAP_ADTYPE_POWER_LEVEL,
      0       // 0dBm
    };
    
    // Advertisement data (max size = 31 bytes, though this is
    // best kept short to conserve power while advertising)
    static uint8_t advertData[] =
    {
      // Flags: this field sets the device to use general discoverable
      // mode (advertises indefinitely) instead of general
      // discoverable mode (advertise for 30 seconds at a time)
      0x02,   // length of this data
      GAP_ADTYPE_FLAGS,
      DEFAULT_DISCOVERABLE_MODE | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,
    
      // service UUID, to notify central devices what services are included
      // in this peripheral
      0x03,   // length of this data
      GAP_ADTYPE_16BIT_MORE,      // some of the UUID's, but not all
      LO_UINT16(SIMPLEPROFILE_SERV_UUID),
      HI_UINT16(SIMPLEPROFILE_SERV_UUID)
    };
    
    // GAP GATT Attributes
    static uint8_t attDeviceName[GAP_DEVICE_NAME_LEN] = "Simple Peripheral";
    
    // Globals used for ATT Response retransmission
    static gattMsgEvent_t *pAttRsp = NULL;
    static uint8_t rspTxRetry = 0;
    
    /*********************************************************************
     * LOCAL FUNCTIONS
     */
    
    static void SimpleBLEPeripheral_init( void );
    static void SimpleBLEPeripheral_taskFxn(UArg a0, UArg a1);
    
    static uint8_t SimpleBLEPeripheral_processStackMsg(ICall_Hdr *pMsg);
    static uint8_t SimpleBLEPeripheral_processGATTMsg(gattMsgEvent_t *pMsg);
    static void SimpleBLEPeripheral_processAppMsg(sbpEvt_t *pMsg);
    static void SimpleBLEPeripheral_processStateChangeEvt(gaprole_States_t newState);
    static void SimpleBLEPeripheral_processCharValueChangeEvt(uint8_t paramID);
    static void SimpleBLEPeripheral_performPeriodicTask(void);
    static void SimpleBLEPeripheral_clockHandler(UArg arg);
    
    static void SimpleBLEPeripheral_sendAttRsp(void);
    static void SimpleBLEPeripheral_freeAttRsp(uint8_t status);
    
    static void SimpleBLEPeripheral_passcodeCB(uint8_t *deviceAddr, uint16_t connHandle,
                                               uint8_t uiInputs, uint8_t uiOutputs);
    static void SimpleBLEPeripheral_pairStateCB(uint16_t connHandle, uint8_t state,
                                             uint8_t status);
    static void SimpleBLEPeripheral_processPairState(uint8_t state, uint8_t status);
    static void SimpleBLEPeripheral_processPasscode(uint8_t uiOutputs);
    
    static void SimpleBLEPeripheral_stateChangeCB(gaprole_States_t newState);
    static void SimpleBLEPeripheral_charValueChangeCB(uint8_t paramID);
    static uint8_t SimpleBLEPeripheral_enqueueMsg(uint8_t event, uint8_t state,
                                                  uint8_t *pData);
    
    /*********************************************************************
     * EXTERN FUNCTIONS
     */
    extern void AssertHandler(uint8 assertCause, uint8 assertSubcause);
    
    /*********************************************************************
     * PROFILE CALLBACKS
     */
    
    // Peripheral GAPRole Callbacks
    static gapRolesCBs_t SimpleBLEPeripheral_gapRoleCBs =
    {
      SimpleBLEPeripheral_stateChangeCB     // GAPRole State Change Callbacks
    };
    
    // GAP Bond Manager Callbacks
    // These are set to NULL since they are not needed. The application
    // is set up to only perform justworks pairing.
    static gapBondCBs_t simpleBLEPeripheral_BondMgrCBs =
    {
      (pfnPasscodeCB_t) SimpleBLEPeripheral_passcodeCB, // Passcode callback
      SimpleBLEPeripheral_pairStateCB                   // Pairing / Bonding state Callback
    };
    
    // Simple GATT Profile Callbacks
    static simpleProfileCBs_t SimpleBLEPeripheral_simpleProfileCBs =
    {
      SimpleBLEPeripheral_charValueChangeCB // Simple GATT Characteristic value change callback
    };
    
    /*********************************************************************
     * PUBLIC FUNCTIONS
     */
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_createTask
     *
     * @brief   Task creation function for the Simple Peripheral.
     *
     * @param   None.
     *
     * @return  None.
     */
    void SimpleBLEPeripheral_createTask(void)
    {
      Task_Params taskParams;
    
      // Configure task
      Task_Params_init(&taskParams);
      taskParams.stack = sbpTaskStack;
      taskParams.stackSize = SBP_TASK_STACK_SIZE;
      taskParams.priority = SBP_TASK_PRIORITY;
    
      Task_construct(&sbpTask, SimpleBLEPeripheral_taskFxn, &taskParams, NULL);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_init
     *
     * @brief   Called during initialization and contains application
     *          specific initialization (ie. hardware initialization/setup,
     *          table initialization, power up notification, etc), and
     *          profile initialization/setup.
     *
     * @param   None.
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_init(void)
    {
      // ******************************************************************
      // N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
      // ******************************************************************
      // Register the current thread as an ICall dispatcher application
      // so that the application can send and receive messages.
      ICall_registerApp(&selfEntity, &syncEvent);
    
    #ifdef USE_RCOSC
      RCOSC_enableCalibration();
    #endif // USE_RCOSC
    
    #if defined( USE_FPGA )
      // configure RF Core SMI Data Link
      IOCPortConfigureSet(IOID_12, IOC_PORT_RFC_GPO0, IOC_STD_OUTPUT);
      IOCPortConfigureSet(IOID_11, IOC_PORT_RFC_GPI0, IOC_STD_INPUT);
    
      // configure RF Core SMI Command Link
      IOCPortConfigureSet(IOID_10, IOC_IOCFG0_PORT_ID_RFC_SMI_CL_OUT, IOC_STD_OUTPUT);
      IOCPortConfigureSet(IOID_9, IOC_IOCFG0_PORT_ID_RFC_SMI_CL_IN, IOC_STD_INPUT);
    
      // configure RF Core tracer IO
      IOCPortConfigureSet(IOID_8, IOC_PORT_RFC_TRC, IOC_STD_OUTPUT);
    #else // !USE_FPGA
      #if defined( DEBUG_SW_TRACE )
        // configure RF Core tracer IO
        IOCPortConfigureSet(IOID_8, IOC_PORT_RFC_TRC, IOC_STD_OUTPUT | IOC_CURRENT_4MA | IOC_SLEW_ENABLE);
      #endif // DEBUG_SW_TRACE
    #endif // USE_FPGA
    
      // Create an RTOS queue for message from profile to be sent to app.
      appMsgQueue = Util_constructQueue(&appMsg);
    
      // Create one-shot clocks for internal periodic events.
      Util_constructClock(&periodicClock, SimpleBLEPeripheral_clockHandler,
                          SBP_PERIODIC_EVT_PERIOD, 0, false, SBP_PERIODIC_EVT);
    
      Util_startClock(&periodicClock);
    
      dispHandle = Display_open(SBP_DISPLAY_TYPE, NULL);
    
      // Set GAP Parameters: After a connection was established, delay in seconds
      // before sending when GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE,...)
      // uses GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS or
      // GAPROLE_LINK_PARAM_UPDATE_INITIATE_APP_PARAMS
      // For current defaults, this has no effect.
      GAP_SetParamValue(TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL);
    
      // Setup the Peripheral GAPRole Profile. For more information see the User's
      // Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html/
      {
        // Device starts advertising upon initialization of GAP
        uint8_t initialAdvertEnable = TRUE;
    
        // By setting this to zero, the device will go into the waiting state after
        // being discoverable for 30.72 second, and will not being advertising again
        // until re-enabled by the application
        uint16_t advertOffTime = 0;
    
        uint8_t enableUpdateRequest = DEFAULT_ENABLE_UPDATE_REQUEST;
        uint16_t desiredMinInterval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
        uint16_t desiredMaxInterval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
        uint16_t desiredSlaveLatency = DEFAULT_DESIRED_SLAVE_LATENCY;
        uint16_t desiredConnTimeout = DEFAULT_DESIRED_CONN_TIMEOUT;
    
        // Set the Peripheral GAPRole Parameters
        GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
                             &initialAdvertEnable);
        GAPRole_SetParameter(GAPROLE_ADVERT_OFF_TIME, sizeof(uint16_t),
                             &advertOffTime);
    
        GAPRole_SetParameter(GAPROLE_SCAN_RSP_DATA, sizeof(scanRspData),
                             scanRspData);
        GAPRole_SetParameter(GAPROLE_ADVERT_DATA, sizeof(advertData), advertData);
    
        GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE, sizeof(uint8_t),
                             &enableUpdateRequest);
        GAPRole_SetParameter(GAPROLE_MIN_CONN_INTERVAL, sizeof(uint16_t),
                             &desiredMinInterval);
        GAPRole_SetParameter(GAPROLE_MAX_CONN_INTERVAL, sizeof(uint16_t),
                             &desiredMaxInterval);
        GAPRole_SetParameter(GAPROLE_SLAVE_LATENCY, sizeof(uint16_t),
                             &desiredSlaveLatency);
        GAPRole_SetParameter(GAPROLE_TIMEOUT_MULTIPLIER, sizeof(uint16_t),
                             &desiredConnTimeout);
      }
    
      // Set the Device Name characteristic in the GAP GATT Service
      // For more information, see the section in the User's Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html
      GGS_SetParameter(GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, attDeviceName);
    
      // Set GAP Parameters to set the advertising interval
      // For more information, see the GAP section of the User's Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html
      {
        // Use the same interval for general and limited advertising.
        // Note that only general advertising will occur based on the above configuration
        uint16_t advInt = DEFAULT_ADVERTISING_INTERVAL;
    
        GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN, advInt);
        GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX, advInt);
        GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN, advInt);
        GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX, advInt);
      }
    
      // Setup the GAP Bond Manager. For more information see the section in the
      // User's Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html/
      {
        // Don't send a pairing request after connecting; the peer device must
        // initiate pairing
        uint8_t pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
        // Use authenticated pairing: require passcode.
        uint8_t mitm = TRUE;
        // This device only has display capabilities. Therefore, it will display the
        // passcode during pairing. However, since the default passcode is being
        // used, there is no need to display anything.
        uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
        // Request bonding (storing long-term keys for re-encryption upon subsequent
        // connections without repairing)
        uint8_t bonding = TRUE;
    
        GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
        GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
        GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);
        GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);
      }
    
      // Initialize GATT attributes
      GGS_AddService(GATT_ALL_SERVICES);           // GAP GATT Service
      GATTServApp_AddService(GATT_ALL_SERVICES);   // GATT Service
      DevInfo_AddService();                        // Device Information Service
    
      // Setup the SimpleProfile Characteristic Values
      // For more information, see the sections in the User's Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html/
      {
        uint8_t charValue1 = 1;
        uint8_t charValue2 = 2;
        uint8_t charValue3 = 3;
        uint8_t charValue4 = 4;
        uint8_t charValue5[SIMPLEPROFILE_CHAR5_LEN] = { 1, 2, 3, 4, 5 };
    
        SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR1, sizeof(uint8_t),
                                   &charValue1);
        SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR2, sizeof(uint8_t),
                                   &charValue2);
        SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR3, sizeof(uint8_t),
                                   &charValue3);
        SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR4, sizeof(uint8_t),
                                   &charValue4);
        SimpleProfile_SetParameter(SIMPLEPROFILE_CHAR5, SIMPLEPROFILE_CHAR5_LEN,
                                   charValue5);
      }
    
      // Register callback with SimpleGATTprofile
      SimpleProfile_RegisterAppCBs(&SimpleBLEPeripheral_simpleProfileCBs);
    
      // Start the Device
      VOID GAPRole_StartDevice(&SimpleBLEPeripheral_gapRoleCBs);
    
      // Start Bond Manager and register callback
      VOID GAPBondMgr_Register(&simpleBLEPeripheral_BondMgrCBs);
    
      // Register with GAP for HCI/Host messages. This is needed to receive HCI
      // events. For more information, see the section in the User's Guide:
      // http://software-dl.ti.com/lprf/sdg-latest/html
      GAP_RegisterForMsgs(selfEntity);
    
      // Register for GATT local events and ATT Responses pending for transmission
      GATT_RegisterForMsgs(selfEntity);
    
      //Set default values for Data Length Extension
      {
        //Set initial values to maximum, RX is set to max. by default(251 octets, 2120us)
        #define APP_SUGGESTED_PDU_SIZE 251 //default is 27 octets(TX)
        #define APP_SUGGESTED_TX_TIME 2120 //default is 328us(TX)
    
        //This API is documented in hci.h
        //See the LE Data Length Extension section in the BLE-Stack User's Guide for information on using this command:
        //http://software-dl.ti.com/lprf/sdg-latest/html/cc2640/index.html
        //HCI_LE_WriteSuggestedDefaultDataLenCmd(APP_SUGGESTED_PDU_SIZE, APP_SUGGESTED_TX_TIME);
      }
    
    #if !defined (USE_LL_CONN_PARAM_UPDATE)
      // Get the currently set local supported LE features
      // The HCI will generate an HCI event that will get received in the main
      // loop
      HCI_LE_ReadLocalSupportedFeaturesCmd();
    #endif // !defined (USE_LL_CONN_PARAM_UPDATE)
    
      Display_print0(dispHandle, 0, 0, "BLE Peripheral");
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_taskFxn
     *
     * @brief   Application task entry point for the Simple Peripheral.
     *
     * @param   a0, a1 - not used.
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_taskFxn(UArg a0, UArg a1)
    {
      // Initialize application
      SimpleBLEPeripheral_init();
    
      // Application main loop
      for (;;)
      {
        uint32_t events;
    
        // Waits for an event to be posted associated with the calling thread.
        // Note that an event associated with a thread is posted when a
        // message is queued to the message receive queue of the thread
        events = Event_pend(syncEvent, Event_Id_NONE, SBP_ALL_EVENTS,
                            ICALL_TIMEOUT_FOREVER);
    
        if (events)
        {
          ICall_EntityID dest;
          ICall_ServiceEnum src;
          ICall_HciExtEvt *pMsg = NULL;
    
          // Fetch any available messages that might have been sent from the stack
          if (ICall_fetchServiceMsg(&src, &dest,
                                    (void **)&pMsg) == ICALL_ERRNO_SUCCESS)
          {
            uint8 safeToDealloc = TRUE;
    
            if ((src == ICALL_SERVICE_CLASS_BLE) && (dest == selfEntity))
            {
              ICall_Stack_Event *pEvt = (ICall_Stack_Event *)pMsg;
    
              // Check for BLE stack events first
              if (pEvt->signature == 0xffff)
              {
                // The GATT server might have returned a blePending as it was trying
                // to process an ATT Response. Now that we finished with this
                // connection event, let's try sending any remaining ATT Responses
                // on the next connection event.
                if (pEvt->event_flag & SBP_HCI_CONN_EVT_END_EVT)
                {
                  // Try to retransmit pending ATT Response (if any)
                  SimpleBLEPeripheral_sendAttRsp();
                }
              }
              else
              {
                // Process inter-task message
                safeToDealloc = SimpleBLEPeripheral_processStackMsg((ICall_Hdr *)pMsg);
              }
            }
    
            if (pMsg && safeToDealloc)
            {
              ICall_freeMsg(pMsg);
            }
          }
    
          // If RTOS queue is not empty, process app message.
          if (events & SBP_QUEUE_EVT)
          {
            while (!Queue_empty(appMsgQueue))
            {
              sbpEvt_t *pMsg = (sbpEvt_t *)Util_dequeueMsg(appMsgQueue);
              if (pMsg)
              {
                // Process message.
                SimpleBLEPeripheral_processAppMsg(pMsg);
    
                // Free the space from the message.
                ICall_free(pMsg);
              }
            }
          }
    
          if (events & SBP_PERIODIC_EVT)
          {
            Util_startClock(&periodicClock);
    
            // Perform periodic application task
            SimpleBLEPeripheral_performPeriodicTask();
          }
        }
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processStackMsg
     *
     * @brief   Process an incoming stack message.
     *
     * @param   pMsg - message to process
     *
     * @return  TRUE if safe to deallocate incoming message, FALSE otherwise.
     */
    static uint8_t SimpleBLEPeripheral_processStackMsg(ICall_Hdr *pMsg)
    {
      uint8_t safeToDealloc = TRUE;
    
      switch (pMsg->event)
      {
        case GATT_MSG_EVENT:
          // Process GATT message
          safeToDealloc = SimpleBLEPeripheral_processGATTMsg((gattMsgEvent_t *)pMsg);
          break;
    
        case HCI_GAP_EVENT_EVENT:
          {
    
            // Process HCI message
            switch(pMsg->status)
            {
              case HCI_COMMAND_COMPLETE_EVENT_CODE:
                // Process HCI Command Complete Event
                {
    
    #if !defined (USE_LL_CONN_PARAM_UPDATE)
                  // This code will disable the use of the LL_CONNECTION_PARAM_REQ
                  // control procedure (for connection parameter updates, the
                  // L2CAP Connection Parameter Update procedure will be used
                  // instead). To re-enable the LL_CONNECTION_PARAM_REQ control
                  // procedures, define the symbol USE_LL_CONN_PARAM_UPDATE
                  // The L2CAP Connection Parameter Update procedure is used to
                  // support a delta between the minimum and maximum connection
                  // intervals required by some iOS devices.
    
                  // Parse Command Complete Event for opcode and status
                  hciEvt_CmdComplete_t* command_complete = (hciEvt_CmdComplete_t*) pMsg;
                  uint8_t   pktStatus = command_complete->pReturnParam[0];
    
                  //find which command this command complete is for
                  switch (command_complete->cmdOpcode)
                  {
                    case HCI_LE_READ_LOCAL_SUPPORTED_FEATURES:
                      {
                        if (pktStatus == SUCCESS)
                        {
                          uint8_t featSet[8];
    
                          // Get current feature set from received event (bits 1-9
                          // of the returned data
                          memcpy( featSet, &command_complete->pReturnParam[1], 8 );
    
                          // Clear bit 1 of byte 0 of feature set to disable LL
                          // Connection Parameter Updates
                          CLR_FEATURE_FLAG( featSet[0], LL_FEATURE_CONN_PARAMS_REQ );
    
                          // Update controller with modified features
                          HCI_EXT_SetLocalSupportedFeaturesCmd( featSet );
                        }
                      }
                      break;
    
                    default:
                      //do nothing
                      break;
                  }
    #endif // !defined (USE_LL_CONN_PARAM_UPDATE)
    
                }
                break;
    
              case HCI_BLE_HARDWARE_ERROR_EVENT_CODE:
                AssertHandler(HAL_ASSERT_CAUSE_HARDWARE_ERROR,0);
                break;
    
              default:
                break;
            }
          }
          break;
    
          default:
            // do nothing
            break;
    
        }
    
      return (safeToDealloc);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processGATTMsg
     *
     * @brief   Process GATT messages and events.
     *
     * @return  TRUE if safe to deallocate incoming message, FALSE otherwise.
     */
    static uint8_t SimpleBLEPeripheral_processGATTMsg(gattMsgEvent_t *pMsg)
    {
      // See if GATT server was unable to transmit an ATT response
      if (pMsg->hdr.status == blePending)
      {
        // No HCI buffer was available. Let's try to retransmit the response
        // on the next connection event.
        if (HCI_EXT_ConnEventNoticeCmd(pMsg->connHandle, selfEntity,
                                       SBP_HCI_CONN_EVT_END_EVT) == SUCCESS)
        {
          // First free any pending response
          SimpleBLEPeripheral_freeAttRsp(FAILURE);
    
          // Hold on to the response message for retransmission
          pAttRsp = pMsg;
    
          // Don't free the response message yet
          return (FALSE);
        }
      }
      else if (pMsg->method == ATT_FLOW_CTRL_VIOLATED_EVENT)
      {
        // ATT request-response or indication-confirmation flow control is
        // violated. All subsequent ATT requests or indications will be dropped.
        // The app is informed in case it wants to drop the connection.
    
        // Display the opcode of the message that caused the violation.
        Display_print1(dispHandle, 5, 0, "FC Violated: %d", pMsg->msg.flowCtrlEvt.opcode);
      }
      else if (pMsg->method == ATT_MTU_UPDATED_EVENT)
      {
        // MTU size updated
        Display_print1(dispHandle, 5, 0, "MTU Size: %d", pMsg->msg.mtuEvt.MTU);
      }
    
      // Free message payload. Needed only for ATT Protocol messages
      GATT_bm_free(&pMsg->msg, pMsg->method);
    
      // It's safe to free the incoming message
      return (TRUE);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_sendAttRsp
     *
     * @brief   Send a pending ATT response message.
     *
     * @param   none
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_sendAttRsp(void)
    {
      // See if there's a pending ATT Response to be transmitted
      if (pAttRsp != NULL)
      {
        uint8_t status;
    
        // Increment retransmission count
        rspTxRetry++;
    
        // Try to retransmit ATT response till either we're successful or
        // the ATT Client times out (after 30s) and drops the connection.
        status = GATT_SendRsp(pAttRsp->connHandle, pAttRsp->method, &(pAttRsp->msg));
        if ((status != blePending) && (status != MSG_BUFFER_NOT_AVAIL))
        {
          // Disable connection event end notice
          HCI_EXT_ConnEventNoticeCmd(pAttRsp->connHandle, selfEntity, 0);
    
          // We're done with the response message
          SimpleBLEPeripheral_freeAttRsp(status);
        }
        else
        {
          // Continue retrying
          Display_print1(dispHandle, 5, 0, "Rsp send retry: %d", rspTxRetry);
        }
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_freeAttRsp
     *
     * @brief   Free ATT response message.
     *
     * @param   status - response transmit status
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_freeAttRsp(uint8_t status)
    {
      // See if there's a pending ATT response message
      if (pAttRsp != NULL)
      {
        // See if the response was sent out successfully
        if (status == SUCCESS)
        {
          Display_print1(dispHandle, 5, 0, "Rsp sent retry: %d", rspTxRetry);
        }
        else
        {
          // Free response payload
          GATT_bm_free(&pAttRsp->msg, pAttRsp->method);
    
          Display_print1(dispHandle, 5, 0, "Rsp retry failed: %d", rspTxRetry);
        }
    
        // Free response message
        ICall_freeMsg(pAttRsp);
    
        // Reset our globals
        pAttRsp = NULL;
        rspTxRetry = 0;
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processAppMsg
     *
     * @brief   Process an incoming callback from a profile.
     *
     * @param   pMsg - message to process
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_processAppMsg(sbpEvt_t *pMsg)
    {
      switch (pMsg->hdr.event)
      {
        case SBP_STATE_CHANGE_EVT:
          {
            SimpleBLEPeripheral_processStateChangeEvt((gaprole_States_t)pMsg->
                                                    hdr.state);
          }
          break;
    
        case SBP_CHAR_CHANGE_EVT:
          {
            SimpleBLEPeripheral_processCharValueChangeEvt(pMsg->hdr.state);
          }
          break;
    
        // Pairing event
        case SBP_PAIRING_STATE_EVT:
          {
            SimpleBLEPeripheral_processPairState(pMsg->hdr.state, *pMsg->pData);
    
            ICall_free(pMsg->pData);
            break;
          }
    
        // Passcode event
        case SBP_PASSCODE_NEEDED_EVT:
          {
            SimpleBLEPeripheral_processPasscode(*pMsg->pData);
    
            ICall_free(pMsg->pData);
            break;
          }
    
        default:
          // Do nothing.
          break;
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_stateChangeCB
     *
     * @brief   Callback from GAP Role indicating a role state change.
     *
     * @param   newState - new state
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_stateChangeCB(gaprole_States_t newState)
    {
      SimpleBLEPeripheral_enqueueMsg(SBP_STATE_CHANGE_EVT, newState, 0);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processStateChangeEvt
     *
     * @brief   Process a pending GAP Role state change event.
     *
     * @param   newState - new state
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_processStateChangeEvt(gaprole_States_t newState)
    {
    #ifdef PLUS_BROADCASTER
      static bool firstConnFlag = false;
    #endif // PLUS_BROADCASTER
    
      switch ( newState )
      {
        case GAPROLE_STARTED:
          {
            uint8_t ownAddress[B_ADDR_LEN];
            uint8_t systemId[DEVINFO_SYSTEM_ID_LEN];
    
            GAPRole_GetParameter(GAPROLE_BD_ADDR, ownAddress);
    
            // use 6 bytes of device address for 8 bytes of system ID value
            systemId[0] = ownAddress[0];
            systemId[1] = ownAddress[1];
            systemId[2] = ownAddress[2];
    
            // set middle bytes to zero
            systemId[4] = 0x00;
            systemId[3] = 0x00;
    
            // shift three bytes up
            systemId[7] = ownAddress[5];
            systemId[6] = ownAddress[4];
            systemId[5] = ownAddress[3];
    
            DevInfo_SetParameter(DEVINFO_SYSTEM_ID, DEVINFO_SYSTEM_ID_LEN, systemId);
    
            // Display device address
            Display_print0(dispHandle, 1, 0, Util_convertBdAddr2Str(ownAddress));
            Display_print0(dispHandle, 2, 0, "Initialized");
          }
          break;
    
        case GAPROLE_ADVERTISING:
          Display_print0(dispHandle, 2, 0, "Advertising");
          break;
    
    #ifdef PLUS_BROADCASTER
        // After a connection is dropped, a device in PLUS_BROADCASTER will continue
        // sending non-connectable advertisements and shall send this change of
        // state to the application.  These are then disabled here so that sending
        // connectable advertisements can resume.
        case GAPROLE_ADVERTISING_NONCONN:
          {
            uint8_t advertEnabled = FALSE;
    
            // Disable non-connectable advertising.
            GAPRole_SetParameter(GAPROLE_ADV_NONCONN_ENABLED, sizeof(uint8_t),
                               &advertEnabled);
    
            advertEnabled = TRUE;
    
            // Enabled connectable advertising.
            GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
                                 &advertEnabled);
    
            // Reset flag for next connection.
            firstConnFlag = false;
    
            SimpleBLEPeripheral_freeAttRsp(bleNotConnected);
          }
          break;
    #endif //PLUS_BROADCASTER
    
        case GAPROLE_CONNECTED:
          {
            linkDBInfo_t linkInfo;
            uint8_t numActive = 0;
    
            numActive = linkDB_NumActive();
    
            // Use numActive to determine the connection handle of the last
            // connection
            if ( linkDB_GetInfo( numActive - 1, &linkInfo ) == SUCCESS )
            {
              Display_print1(dispHandle, 2, 0, "Num Conns: %d", (uint16_t)numActive);
              Display_print0(dispHandle, 3, 0, Util_convertBdAddr2Str(linkInfo.addr));
            }
            else
            {
              uint8_t peerAddress[B_ADDR_LEN];
    
              GAPRole_GetParameter(GAPROLE_CONN_BD_ADDR, peerAddress);
    
              Display_print0(dispHandle, 2, 0, "Connected");
              Display_print0(dispHandle, 3, 0, Util_convertBdAddr2Str(peerAddress));
            }
    
            #ifdef PLUS_BROADCASTER
              // Only turn advertising on for this state when we first connect
              // otherwise, when we go from connected_advertising back to this state
              // we will be turning advertising back on.
              if (firstConnFlag == false)
              {
                uint8_t advertEnabled = FALSE; // Turn on Advertising
    
                // Disable connectable advertising.
                GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
                                     &advertEnabled);
    
                // Set to true for non-connectable advertising.
                advertEnabled = TRUE;
    
                // Enable non-connectable advertising.
                GAPRole_SetParameter(GAPROLE_ADV_NONCONN_ENABLED, sizeof(uint8_t),
                                     &advertEnabled);
                firstConnFlag = true;
              }
            #endif // PLUS_BROADCASTER
          }
          break;
    
        case GAPROLE_CONNECTED_ADV:
          Display_print0(dispHandle, 2, 0, "Connected Advertising");
          break;
    
        case GAPROLE_WAITING:
          Util_stopClock(&periodicClock);
          SimpleBLEPeripheral_freeAttRsp(bleNotConnected);
    
          Display_print0(dispHandle, 2, 0, "Disconnected");
    
          // Clear remaining lines
          Display_clearLines(dispHandle, 3, 5);
          break;
    
        case GAPROLE_WAITING_AFTER_TIMEOUT:
          SimpleBLEPeripheral_freeAttRsp(bleNotConnected);
    
          Display_print0(dispHandle, 2, 0, "Timed Out");
    
          // Clear remaining lines
          Display_clearLines(dispHandle, 3, 5);
    
          #ifdef PLUS_BROADCASTER
            // Reset flag for next connection.
            firstConnFlag = false;
          #endif // PLUS_BROADCASTER
          break;
    
        case GAPROLE_ERROR:
          Display_print0(dispHandle, 2, 0, "Error");
          break;
    
        default:
          Display_clearLine(dispHandle, 2);
          break;
      }
    
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_charValueChangeCB
     *
     * @brief   Callback from Simple Profile indicating a characteristic
     *          value change.
     *
     * @param   paramID - parameter ID of the value that was changed.
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_charValueChangeCB(uint8_t paramID)
    {
      SimpleBLEPeripheral_enqueueMsg(SBP_CHAR_CHANGE_EVT, paramID, 0);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processCharValueChangeEvt
     *
     * @brief   Process a pending Simple Profile characteristic value change
     *          event.
     *
     * @param   paramID - parameter ID of the value that was changed.
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_processCharValueChangeEvt(uint8_t paramID)
    {
      uint8_t newValue;
    
      switch(paramID)
      {
        case SIMPLEPROFILE_CHAR1:
          SimpleProfile_GetParameter(SIMPLEPROFILE_CHAR1, &newValue);
    
          Display_print1(dispHandle, 4, 0, "Char 1: %d", (uint16_t)newValue);
          break;
    
        case SIMPLEPROFILE_CHAR3:
          SimpleProfile_GetParameter(SIMPLEPROFILE_CHAR3, &newValue);
    
          Display_print1(dispHandle, 4, 0, "Char 3: %d", (uint16_t)newValue);
          break;
    
        default:
          // should not reach here!
          break;
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_performPeriodicTask
     *
     * @brief   Perform a periodic application task. This function gets called
     *          every five seconds (SBP_PERIODIC_EVT_PERIOD). In this example,
     *          the value of the third characteristic in the SimpleGATTProfile
     *          service is retrieved from the profile, and then copied into the
     *          value of the the fourth characteristic.
     *
     * @param   None.
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_performPeriodicTask(void)
    {
      // Perform periodic application task
      static uint8_t status = 1;
      uint16_t handle = 0;
      uint8 apiStat = SUCCESS;
      if (status == 1)
      {
        status = 0;
        apiStat = SimpleProfile_AddService(GATT_ALL_SERVICES);
        Display_printf(dispHandle, 5, 0,
                       "Service Registered with %d stat",
                       apiStat);
    
      }
      else
      {
        status = 1;
        handle = SimpleProfile_RemoveService();
        Display_printf(dispHandle, 6, 0,
                       "Service Deregistered with handle: %d",
                       handle);
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_pairStateCB
     *
     * @brief   Pairing state callback.
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_pairStateCB(uint16_t connHandle, uint8_t state,
                                                uint8_t status)
    {
      uint8_t *pData;
    
      // Allocate space for the event data.
      if ((pData = ICall_malloc(sizeof(uint8_t))))
      {
        *pData = status;
    
        // Queue the event.
        SimpleBLEPeripheral_enqueueMsg(SBP_PAIRING_STATE_EVT, state, pData);
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processPairState
     *
     * @brief   Process the new paring state.
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_processPairState(uint8_t state, uint8_t status)
    {
      if (state == GAPBOND_PAIRING_STATE_STARTED)
      {
        Display_print0(dispHandle, 2, 0, "Pairing started");
      }
      else if (state == GAPBOND_PAIRING_STATE_COMPLETE)
      {
        if (status == SUCCESS)
        {
          Display_print0(dispHandle, 2, 0, "Pairing success");
        }
        else
        {
          Display_print1(dispHandle, 2, 0, "Pairing fail: %d", status);
        }
      }
      else if (state == GAPBOND_PAIRING_STATE_BONDED)
      {
        if (status == SUCCESS)
        {
          Display_print0(dispHandle, 2, 0, "Bonding success");
        }
      }
      else if (state == GAPBOND_PAIRING_STATE_BOND_SAVED)
      {
        if (status == SUCCESS)
        {
          Display_print0(dispHandle, 2, 0, "Bond save success");
        }
        else
        {
          Display_print1(dispHandle, 2, 0, "Bond save failed: %d", status);
        }
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_passcodeCB
     *
     * @brief   Passcode callback.
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_passcodeCB(uint8_t *deviceAddr, uint16_t connHandle,
                                               uint8_t uiInputs, uint8_t uiOutputs)
    {
      uint8_t *pData;
    
      // Allocate space for the passcode event.
      if ((pData = ICall_malloc(sizeof(uint8_t))))
      {
        *pData = uiOutputs;
    
        // Enqueue the event.
        SimpleBLEPeripheral_enqueueMsg(SBP_PASSCODE_NEEDED_EVT, 0, pData);
      }
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_processPasscode
     *
     * @brief   Process the Passcode request.
     *
     * @return  none
     */
    static void SimpleBLEPeripheral_processPasscode(uint8_t uiOutputs)
    {
      // This app uses a default passcode. A real-life scenario would handle all
      // pairing scenarios and likely generate this randomly.
      uint32_t passcode = B_APP_DEFAULT_PASSCODE;
    
      // Display passcode to user
      if (uiOutputs != 0)
      {
        Display_print1(dispHandle, 4, 0, "Passcode: %d", passcode);
      }
    
      uint16_t connectionHandle;
      GAPRole_GetParameter(GAPROLE_CONNHANDLE, &connectionHandle);
    
      // Send passcode response
      GAPBondMgr_PasscodeRsp(connectionHandle, SUCCESS, passcode);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_clockHandler
     *
     * @brief   Handler function for clock timeouts.
     *
     * @param   arg - event type
     *
     * @return  None.
     */
    static void SimpleBLEPeripheral_clockHandler(UArg arg)
    {
      // Wake up the application.
      Event_post(syncEvent, arg);
    }
    
    /*********************************************************************
     * @fn      SimpleBLEPeripheral_enqueueMsg
     *
     * @brief   Creates a message and puts the message in RTOS queue.
     *
     * @param   event - message event.
     * @param   state - message state.
     * @param   pData - message data pointer.
     *
     * @return  TRUE or FALSE
     */
    static uint8_t SimpleBLEPeripheral_enqueueMsg(uint8_t event, uint8_t state,
                                               uint8_t *pData)
    {
      sbpEvt_t *pMsg = ICall_malloc(sizeof(sbpEvt_t));
    
      // Create dynamic pointer to message.
      if (pMsg)
      {
        pMsg->hdr.event = event;
        pMsg->hdr.state = state;
        pMsg->pData = pData;
    
        // Enqueue the message.
        return Util_enqueueMsg(appMsgQueue, syncEvent, (uint8_t *)pMsg);
      }
    
      return FALSE;
    }
    /*********************************************************************
    *********************************************************************/