Part Number: CC2642R
Customer is working with Extended Advertising on the CC26x2 Launchpad. There seems to be a difference in the advertising lengths depending on if the advertisement is configured as scannable or connectable.
The advertisement data is a static 300 byte array. When the advertisement is scannable, BTool shows all 300 bytes split between two separate events. However, the data is truncated to 245 bytes when the advertisement is connectable.
Can the advertisement be more than 245 bytes when it is configured as connectable?
Thanks,
Mark