This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Iphone X connection Issues

Part Number: CC2640R2F

Hello,

We have the CC2640R2F chip on a custom board. We are having trouble connecting to our device from an Iphone X. We can discover the device, but it hangs on discovering services (using BLE scanner). We do not have this issue on Ipad Air 2, Iphone 6s, Galaxy S7, Nexus, and Pixel. Has anyone else had issues connecting the CC2640R2F with this particular phone? Is it a heap size issue? Does the Iphone X require more heap to connect?

Where would I begin debugging this issue? Any help would be much appreciated!

We are using CCS 7.4.0.00015, CC2640R2 SDK v:1.50.00.58. We have a total of one custom service with 4 different characteristics. 

Thanks,

Tyler