I am trying to observe the packet stream between a low cost BLE POS receipt printer and a Bluetooth radio USB adapter on a PC. This is a clean RF environment with no other 2.4GHz sources. I am using two PCs for my testing. PC A contains the radio and Teraterm software to send data to the printer. PC B contains the CC2540EMK-USB and your sniffer software V2.18.1. Both PCs are running Windows 7 64bit Pro. The PCs are located about 2 M from each other the printer is located next to PC B. The printer works fine and properly prints data strings entered via Teraterm.
From an earlier post that reported this problem I have set the initiator address in the Radio Configuration tab to PC A radio MAC address to no avail. I only receive advertising packets. I created a filter file to limit the packets displayed but when it is active, no packets are displayed. The file content is as follows.
[LM58]
AA4=0x001A7DDA7113
SA1=0x001A7DDA7113
AA5=0x001A7DDA7113
AA6=0x001A7DDA7113
IA2=0x001A7DDA7113
PTY=0x001A7DDA7113
I have also used the printer MAC address also to no avail. What am I doing wrong?
Best regards,
Al